This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7792 [16 Feb 2012 13:14] – Added the functions' description. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7792 [24 Feb 2012 08:36] – Added the "Reference Project Overview" section. Dragos Bogdan | ||
---|---|---|---|
Line 74: | Line 74: | ||
{{ : | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | |||
+ | The demo program samples channel 1 at 16.7 Hz. The ADC is configured to work in bipolar mode and the gain of the In-Amp is set to 1. The hex values of the configuration and data registers are displayed on the LCD. The value of the Data register is also formatted to be displayed in mV. | ||
+ | |||
{{ : | {{ : | ||