This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:renesas:ad7303 [22 Mar 2012 13:09] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7303 [24 Jan 2021 17:51] (current) – Fix bad links Dragos Bogdan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD7303 - Microcontroller | + | ====== AD7303 - No-OS Driver |
+ | {{page>: | ||
- | ===== Supported Devices ===== | + | **HW Platform(s): |
- | * [[adi> | + | * [[https:// |
+ | * [[https:// | ||
- | ===== Evaluation Boards | + | ===== Downloads |
- | * PmodDA1 | + | |
- | ===== Overview ===== | + | <WRAP round download 80%> |
- | The [[adi>AD7303]] is a dual, 8-bit voltage out DAC that operates from a single +2.7 V to +5.5 V supply. Its on-chip precision output buffers allow the DAC outputs to swing rail to rail. This device uses a versatile 3-wire serial interface that operates at clock rates up to 30 MHz, and is compatible with QSPI, SPI, microwire and digital signal processor interface standards. The serial input register is sixteen bits wide; 8 bits act as data bits for the DACs, and the remaining eight bits make up a control register. | + | * {{: |
+ | * {{: | ||
+ | * {{: | ||
+ | * **AD7303 Driver: | ||
+ | * **PmodDA1 Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
+ | </ | ||
- | {{ : | + | ====== Renesas RL78G13 Quick Start Guide ====== |
+ | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RL78G13 platform. | ||
- | The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers | + | ==== Required Hardware ==== |
+ | * [[https:// | ||
+ | * [[http:// | ||
- | **HW Platform(s): | + | ==== Required Software ==== |
- | * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/ | + | * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench |
- | ===== Driver Description ===== | + | ==== Hardware Setup ==== |
- | The driver contains two parts: | + | A PmodDA1 has to be connected |
- | * The driver for the AD7303 part, which may be used, without modifications, | + | |
- | * The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements | + | |
- | The Communication Driver has a standard interface, so the AD7303 driver can be used exactly as it is provided. | + | {{ : |
- | There are three functions which are called by the AD7303 driver: | + | ==== Reference Project Overview ==== |
- | * SPI_Init() – initializes the communication peripheral. | + | The reference project: |
- | * SPI_Write() – writes data to the device. | + | * outputs a 3 Hz sine wave on channel A; |
- | * SPI_Read() – reads data from the device. | + | * outputs a specific value(zero scale, middle scale and full scale) every second on channel B. |
- | {{ : | ||
- | <WRAP centeralign> | ||
- | SPI driver architecture | ||
- | </ | ||
- | The following functions are implemented in this version of AD7303 driver: | + | {{ :resources: |
- | ^ Function | + | |
- | | unsigned char AD7303_Init(void) | Initializes the SPI communication peripheral. | | + | |
- | | void AD7303_Write(unsigned char controlReg, unsigned char dataReg) | Sends data to AD7303. | | + | |
- | ===== Downloads | + | ==== Software Project Tutorial |
- | * {{: | + | {{page> |
- | | + | |
- | ====== Renesas | + | ====== Renesas |
- | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas | + | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
- | * PmodDA1 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http://am.renesas.com/ | + | * The AD7303 demonstration project for the Renesas RL78G14 platform. |
+ | <WRAP round info 80%> | ||
+ | The AD7303 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD7303 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A PmodDA1 has to be connected to the PMOD1 connector. | + | A PmodDA1 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). |
- | {{ : | + | {{ : |
- | ==== Software Setup ==== | + | ==== Reference Project Overview |
- | With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured: | + | The reference project: |
+ | | ||
+ | | ||
- | === CSI10 (Clocked Serial Interface 10) – For the AD7303 part and the ST7579 LCD === | + | {{ :resources:tools-software:uc-drivers:renesas:pmod_da1_rl78g14_screen.jpg? |}} |
- | Choose to generate the Transmit/ | + | |
- | * Transfer mode setting: //**Single transfer mode**// | + | |
- | * Data length setting | + | |
- | * Transfer direction setting: // | + | |
- | * Specification of data timing: //**Type 1**// | + | |
- | * Transfer rate setting – Clock mode: // | + | |
- | * Transfer rate setting – Baudrate: // | + | |
- | * Interrupt setting – Transfer interrupt priority (INTCSI10): // | + | |
- | * Uncheck the callback functions. | + | |
- | === TM00 (Timer 00) – For the DelayMs() function === | ||
- | Configure TM00 as an interval timer: | ||
- | * Interval timer setting - Interval value(16 bits): //**1**// ms | ||
- | * Interval timer setting - Uncheck //Generates INTM00 when counting is started// | ||
- | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | ||
- | === Watchdog Timer === | + | ==== Software Project Tutorial ==== |
- | Disable | + | {{page> |
- | * Choose | + | |
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[https:// | ||
+ | * [[http://www.digilentinc.com/ | ||
+ | ==== Required Software ==== | ||
+ | | ||
+ | | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodAD5 has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | PmodDA1 Pin 1 (CS) → YRDKRX62N J8 connector Pin 15 | ||
+ | PmodDA1 Pin 2 (MOSI) → YRDKRX62N J8 connector Pin 19 | ||
+ | PmodDA1 Pin 4 (CLK) → YRDKRX62N J8 connector Pin 20 | ||
+ | PmodDA1 Pin 5 (GND) → YRDKRX62N J8 connector Pin 4 | ||
+ | PmodDA1 Pin 6 (VCC) → YRDKRX62N J8 connector Pin 3 | ||
+ | |||
+ | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
The reference project outputs a 3 Hz sinewave on channel A and a specific value every second on channel B. | The reference project outputs a 3 Hz sinewave on channel A and a specific value every second on channel B. | ||
- | {{ : | + | {{ : |
- | + | ||
- | ==== Software Project Tutorial ==== | + | |
- | {{page> | + | |
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | ====== More information ====== | ||
+ | {{page>: |