This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7303 [06 Nov 2012 14:40] – Removed applilet3 content / updated drivers. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7303 [22 Jul 2019 13:52] – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **AD7303 Driver: | ||
+ | * **PmodDA1 Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 25: | Line 28: | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A PmodDA1 has to be connected to the PMOD1 connector. | + | A PmodDA1 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). |
{{ : | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project outputs a 3 Hz sine wave on channel A and a specific value every second on channel B. | + | The reference project: |
+ | * outputs a 3 Hz sine wave on channel A; | ||
+ | * outputs | ||
{{ : | {{ : | ||
Line 36: | Line 42: | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RL78G14 platform using the PmodDA1. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The AD7303 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD7303 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD7303 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDA1 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | * outputs a 4 Hz sine wave on channel A; | ||
+ | * outputs a specific value(zero scale, middle scale and full scale) every second on channel B. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |