This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7303 [11 Jul 2012 09:10] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7303 [19 Jul 2012 13:59] – [Downloads] Dragos Bogdan | ||
---|---|---|---|
Line 18: | Line 18: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 46: | Line 47: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RL78G13 platform. | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RL78G13 platform. | ||
Line 129: | Line 130: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodDA1 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
Line 160: | Line 161: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: | ||
+ | |||
+ | ====== Digilent Cerebot MC7 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD7303 demonstration project on a Digilent Cerebot MC7 platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDA1 has to be connected to the JB connector of Cerebot MC7 development board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | Following commands were implemented in this version of AD7303 reference project for Cerebot MC7 board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | help? | Displays all available commands. | | ||
+ | | power= | Powers off/on the current channel. Accepted values: 0, 1. | | ||
+ | | power? | Displays the power status. | | ||
+ | | channel= | Selects a channel. Accepted values: 0, 1. | | ||
+ | | channel? | Displays the current channel. | | ||
+ | | voltage= | Sets the output voltage of the current channel. Accepted values: 0->3.3 | | ||
+ | | voltage? | Displays last written value. | | ||
+ | | register= | Writes to the DAC register of the current channel. Accepted values: 0 - 255. | | ||
+ | | register? | Displays last written value. | | ||
+ | |||
+ | Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A. | ||
+ | |||
+ | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page>: | ||
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |