This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7303 [22 Mar 2012 13:09] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7303 [23 Mar 2012 22:37] – Approved Dragos Bogdan | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * PmodDA1 | + | * [[http:// |
===== Overview ===== | ===== Overview ===== | ||
Line 16: | Line 16: | ||
**HW Platform(s): | **HW Platform(s): | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
The driver contains two parts: | The driver contains two parts: | ||
Line 48: | Line 48: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodDA1 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
Line 91: | Line 91: | ||
{{page> | {{page> | ||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD7303 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodAD5 has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | PmodAD5 Pin 1 (CS) → YRDKRX62N J8 connector Pin 15 | ||
+ | PmodAD5 Pin 2 (MOSI) → YRDKRX62N J8 connector Pin 19 | ||
+ | PmodAD5 Pin 4 (CLK) → YRDKRX62N J8 connector Pin 20 | ||
+ | PmodAD5 Pin 5 (GND) → YRDKRX62N J8 connector Pin 4 | ||
+ | PmodAD5 Pin 6 (VCC) → YRDKRX62N J8 connector Pin 3 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project outputs a 3 Hz sinewave on channel A and a specific value every second on channel B. | ||
+ | |||
+ | {{ : | ||
+ | ==== Software Project Setup ==== | ||
+ | {{page> |