This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7303 [24 Jul 2012 11:26] – Added arduino zip file. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7303 [06 Nov 2012 14:40] – Removed applilet3 content / updated drivers. Dragos Bogdan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD7303 - Microcontroller | + | ====== AD7303 - No-OS Driver |
- | + | {{page>: | |
- | ===== Supported Devices ===== | + | |
- | * [[adi> | + | |
- | + | ||
- | ===== Evaluation Boards ===== | + | |
- | * [[http:// | + | |
- | + | ||
- | ===== Overview ===== | + | |
- | The [[adi> | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms. | + | |
**HW Platform(s): | **HW Platform(s): | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | ===== Driver Description | + | ===== Downloads |
- | The driver contains two parts: | + | |
- | * The driver for the AD7303 part, which may be used, without modifications, | + | |
- | * The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements the communication with the device and hides the actual details of the communication protocol to the ADI driver. | + | |
- | The Communication Driver has a standard interface, so the AD7303 driver can be used exactly as it is provided. | + | < |
- | + | * {{: | |
- | There are three functions which are called by the AD7303 driver: | + | |
- | * SPI_Init() – initializes the communication peripheral. | + | |
- | * SPI_Write() – writes data to the device. | + | |
- | * SPI_Read() – reads data from the device. | + | |
- | + | ||
- | {{ : | + | |
- | < | + | |
- | SPI driver architecture | + | |
- | </ | + | |
- | + | ||
- | The following functions are implemented in this version of AD7303 driver: | + | |
- | ^ Function | + | |
- | | unsigned char AD7303_Init(void) | Initializes the SPI communication peripheral. | | + | |
- | | void AD7303_Write(unsigned char controlReg, unsigned char dataReg) | Sends data to AD7303. | | + | |
- | + | ||
- | ===== Downloads ===== | + | |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
- | * {{: | + | </ |
- | * {{: | + | |
- | * {{: | + | |
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 59: | Line 23: | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 65: | Line 28: | ||
{{ : | {{ : | ||
- | |||
- | ==== Software Setup ==== | ||
- | With the // | ||
- | |||
- | === CSI10 (Clocked Serial Interface 10) – For the AD7303 part and the ST7579 LCD === | ||
- | Choose to generate the Transmit/ | ||
- | * Transfer mode setting: //**Single transfer mode**// | ||
- | * Data length setting : //**8 bits**// | ||
- | * Transfer direction setting: //**MSB**// | ||
- | * Specification of data timing: //**Type 1**// | ||
- | * Transfer rate setting – Clock mode: // | ||
- | * Transfer rate setting – Baudrate: // | ||
- | * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// | ||
- | * Uncheck the callback functions. | ||
- | |||
- | === TM00 (Timer 00) – For the DelayMs() function === | ||
- | Configure TM00 as an interval timer: | ||
- | * Interval timer setting - Interval value(16 bits): //**1**// ms | ||
- | * Interval timer setting - Uncheck //Generates INTM00 when counting is started// | ||
- | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | ||
- | |||
- | === Watchdog Timer === | ||
- | Disable the watchdog timer: | ||
- | * Choose for the Watchdog timer operation setting: // | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project outputs a 3 Hz sinewave | + | The reference project outputs a 3 Hz sine wave on channel A and a specific value every second on channel B. |
{{ : | {{ : | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
- | {{page>rl78g13_software_tutorial}} | + | {{page>rl78g13_software_tutorial_without_applilet3}} |
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== | ||
Line 126: | Line 65: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
- | |||
- | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
- | This section contains a description of the steps required to run the AD7303 demonstration project on a Digilent Cerebot MX3cK platform. | ||
- | |||
- | ==== Required Hardware ==== | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | |||
- | ==== Required Software ==== | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | |||
- | ==== Hardware Setup ==== | ||
- | A PmodDA1 has to be connected to the JE connector of Cerebot MX3cK development board. | ||
- | |||
- | {{ : | ||
- | |||
- | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD7303 reference project for Cerebot MX3cK board. | ||
- | ^ Command ^ Description ^ | ||
- | | help? | Displays all available commands. | | ||
- | | power= | Powers off/on the current channel. Accepted values: 0, 1. | | ||
- | | power? | Displays the power status. | | ||
- | | channel= | Selects a channel. Accepted values: 0, 1. | | ||
- | | channel? | Displays the current channel. | | ||
- | | voltage= | Sets the output voltage of the current channel. Accepted values: 0->3.3 | | ||
- | | voltage? | Displays last written value. | | ||
- | | register= | Writes to the DAC register of the current channel. Accepted values: 0 - 255. | | ||
- | | register? | Displays last written value. | | ||
- | |||
- | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | |||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
- | {{ : | ||
- | |||
- | ==== Software Project Setup ==== | ||
- | {{page>: | ||
- | |||
- | ====== Digilent Cerebot MC7 Quick Start Guide ====== | ||
- | This section contains a description of the steps required to run the AD7303 demonstration project on a Digilent Cerebot MC7 platform. | ||
- | |||
- | ==== Required Hardware ==== | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | |||
- | ==== Required Software ==== | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | |||
- | ==== Hardware Setup ==== | ||
- | A PmodDA1 has to be connected to the JB connector of Cerebot MC7 development board. | ||
- | |||
- | {{ : | ||
- | |||
- | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD7303 reference project for Cerebot MC7 board. | ||
- | ^ Command ^ Description ^ | ||
- | | help? | Displays all available commands. | | ||
- | | power= | Powers off/on the current channel. Accepted values: 0, 1. | | ||
- | | power? | Displays the power status. | | ||
- | | channel= | Selects a channel. Accepted values: 0, 1. | | ||
- | | channel? | Displays the current channel. | | ||
- | | voltage= | Sets the output voltage of the current channel. Accepted values: 0->3.3 | | ||
- | | voltage? | Displays last written value. | | ||
- | | register= | Writes to the DAC register of the current channel. Accepted values: 0 - 255. | | ||
- | | register? | Displays last written value. | | ||
- | |||
- | Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A. | ||
- | |||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
- | {{ : | ||
- | |||
- | ==== Software Project Setup ==== | ||
- | {{page>: | ||
- | |||
- | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino ====== | ||
- | This section contains a description of the steps required to run the AD7303 Arduino demonstration project on a Digilent Cerebot MX3cK platform. | ||
- | |||
- | ==== Required Hardware ==== | ||
- | * [[http:// | ||
- | * PmodDA1 | ||
- | |||
- | ==== Required Software ==== | ||
- | * [[https:// | ||
- | |||
- | ==== Hardware Setup ==== | ||
- | A PmodDA1 has to be connected to the JE connector of Cerebot MX3cK development board. | ||
- | |||
- | {{ : | ||
- | |||
- | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD7303 Arduino reference project for Cerebot MX3cK board. | ||
- | ^ Command ^ Description ^ | ||
- | | help? | Displays all available commands. | | ||
- | | power= | Powers off/on the current channel. Accepted values: 0, 1. | | ||
- | | power? | Displays the power status. | | ||
- | | channel= | Selects a channel. Accepted values: 0, 1. | | ||
- | | channel? | Displays the current channel. | | ||
- | | voltage= | Sets the output voltage of the current channel. Accepted values: 0->3.3 | | ||
- | | voltage? | Displays last written value. | | ||
- | | register= | Writes to the DAC register of the current channel. Accepted values: 0 - 255. | | ||
- | | register? | Displays last written value. | | ||
- | |||
- | Commands can be executed using the serial monitor. | ||
- | |||
- | // | ||
- | |||
- | The following image shows a list of commands in the serial monitor. | ||
- | |||
- | {{ : | ||
- | |||
- | ==== Software Project Setup ==== | ||
- | {{page>: | ||
- | |||
====== More information ====== | ====== More information ====== | ||
- | {{page> | + | {{page>: |