Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:ad7190 [09 Oct 2012 10:26] – Replaced the Overview Section. Dragos Bogdanresources:tools-software:uc-drivers:renesas:ad7190 [25 Jan 2021 05:24] (current) – update renesas links after their web site update Robin Getz
Line 20: Line 20:
 The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms. The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms.
  
-**HW Platform(s):** 
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] 
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] 
 ===== Driver Description ===== ===== Driver Description =====
 The driver contains two parts: The driver contains two parts:
Line 54: Line 51:
 | unsigned long AD7190_ContinuousReadAvg(unsigned char sampleNumber) | Returns the average of several conversion results. | | unsigned long AD7190_ContinuousReadAvg(unsigned char sampleNumber) | Returns the average of several conversion results. |
 | unsigned long AD7190_TemperatureRead(void) | Read data from temperature sensor and converts it to Celsius degrees. | | unsigned long AD7190_TemperatureRead(void) | Read data from temperature sensor and converts it to Celsius degrees. |
 +
 +**HW Platform(s):**
 +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]]
 +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
  
 ===== Downloads ===== ===== Downloads =====
 +
 +<WRAP round download 80%>
   * {{:resources:tools-software:uc-drivers:renesas:ad7190_generic.zip|AD7190 Generic Driver}}   * {{:resources:tools-software:uc-drivers:renesas:ad7190_generic.zip|AD7190 Generic Driver}}
   * {{:resources:tools-software:uc-drivers:renesas:ad7190_rl78g13.zip|AD7190 RL78G13 Driver}}   * {{:resources:tools-software:uc-drivers:renesas:ad7190_rl78g13.zip|AD7190 RL78G13 Driver}}
   * {{:resources:tools-software:uc-drivers:renesas:ad7190_rx62n.zip|AD7190 RX62N Driver}}   * {{:resources:tools-software:uc-drivers:renesas:ad7190_rx62n.zip|AD7190 RX62N Driver}}
 +</WRAP>
 +
 ====== Renesas RL78G13 Quick Start Guide ====== ====== Renesas RL78G13 Quick Start Guide ======
 This section contains a description of the steps required to run the AD7190 demonstration project on a Renesas RL78G13 platform.  This section contains a description of the steps required to run the AD7190 demonstration project on a Renesas RL78G13 platform. 
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] 
-  * [[adi>EVAL-AD7190EBZ (Analog Devices)]] +  * [[adi>EVAL-AD7190EBZ|EVAL-AD7190EBZ (Analog Devices)]]
 ==== Required Software ==== ==== Required Software ====
   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
-  * [[http://am.renesas.com/|Applilet3 for RL78G13]] 
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 80: Line 83:
          
 {{ :resources:tools-software:uc-drivers:renesas:eval_ad7190ebz_rl78g13.jpg? |}} {{ :resources:tools-software:uc-drivers:renesas:eval_ad7190ebz_rl78g13.jpg? |}}
- 
-==== Software Setup ==== 
-With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured: 
- 
-=== CSI10 (Clocked Serial Interface 10) – For the AD7190 part and the ST7579 LCD === 
-Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings: 
-  * Transfer mode setting: //**Single transfer mode**// 
-  * Data length setting : //**8 bits**// 
-  * Transfer direction setting: //**MSB**// 
-  * Specification of data timing: //**Type 1**// 
-  * Transfer rate setting – Clock mode: //**Internal clock (master)**// 
-  * Transfer rate setting – Baudrate: //**1000000**// (bps) 
-  * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// 
-  * Uncheck the callback functions. 
- 
-=== TM00 (Timer 00) – For the DelayMs() function ===  
-Configure TM00 as an interval timer: 
-  * Interval timer setting - Interval value(16 bits): //**1**// ms 
-  * Interval timer setting - Uncheck //Generates INTM00 when counting is started// 
-  * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// 
- 
-=== Watchdog Timer === 
-Disable the watchdog timer: 
-  * Choose for the Watchdog timer operation setting: //**Unused**// option. 
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
Line 117: Line 96:
  
 ==== Software Project Setup ==== ==== Software Project Setup ====
-{{page>rl78g13_software_tutorial}}+{{page>rl78g13_software_tutorial_without_applilet3}}
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
Line 124: Line 103:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
   * [[adi>EVAL-AD7190EBZ|EVAL-AD7190EBZ (ADI)]]   * [[adi>EVAL-AD7190EBZ|EVAL-AD7190EBZ (ADI)]]
  
 ==== Required Software ==== ==== Required Software ====
-  * [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]]+  * [[https://www.renesas.com/us/en/software-tool/high-performance-embedded-workshop|High-performance Embedded Workshop for RX62N family]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
resources/tools-software/uc-drivers/renesas/ad7190.txt · Last modified: 25 Jan 2021 05:24 by Robin Getz