This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7176 [04 Dec 2012 14:10] – Added a picture of the evaluation board. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7176 [20 Dec 2012 09:52] – Added reset function. Dan Nechita | ||
---|---|---|---|
Line 52: | Line 52: | ||
| int32_t AD7176_ReadRegister(st_reg* pReg) | Reads the value of the specified register. | | | int32_t AD7176_ReadRegister(st_reg* pReg) | Reads the value of the specified register. | | ||
| int32_t AD7176_WriteRegister(st_reg reg) | Writes the value of the specified register. | | | int32_t AD7176_WriteRegister(st_reg reg) | Writes the value of the specified register. | | ||
+ | | int32_t AD7176_Reset(void) | Resets the device. | | ||
| int32_t AD7176_WaitForReady(uint32_t timeout) | Waits until a new conversion result is available. | | | int32_t AD7176_WaitForReady(uint32_t timeout) | Waits until a new conversion result is available. | | ||
| int32_t AD7176_ReadData(int32_t* pData) | Reads the conversion result from the device. | | | int32_t AD7176_ReadData(int32_t* pData) | Reads the conversion result from the device. | | ||
Line 60: | Line 61: | ||
===== Downloads ===== | ===== Downloads ===== | ||
+ | |||
+ | <WRAP round download 30%> | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | </ | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 81: | Line 85: | ||
EVAL-AD7176-2SDZ Pin TSCLK -> YRDKRL78G13 J11 connector Pin 4 | EVAL-AD7176-2SDZ Pin TSCLK -> YRDKRL78G13 J11 connector Pin 4 | ||
EVAL-AD7176-2SDZ Pin GND1 | EVAL-AD7176-2SDZ Pin GND1 | ||
+ | |||
+ | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== |