This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
resources:tools-software:uc-drivers:renesas:ad7176 [04 Dec 2012 11:18] – Created Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7176 [04 Dec 2012 14:10] – Added a picture of the evaluation board. Dragos Bogdan | ||
---|---|---|---|
Line 23: | Line 23: | ||
* Medical and scientific multichannel instrumentation | * Medical and scientific multichannel instrumentation | ||
* Chromatography | * Chromatography | ||
+ | |||
+ | {{ : | ||
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms. | The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms. |