This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7156 [13 Nov 2012 15:15] – Added the round download indicator. Dan Nechita | resources:tools-software:uc-drivers:renesas:ad7156 [26 Apr 2013 15:49] – [Downloads] Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
Line 34: | Line 34: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project samples the input capacitance on both channels and simultaneously checks if any of the two buttons are pressed or released. The two horizontal bars show how much pressure is applied on the two buttons on the pmod. | + | The reference project samples the input capacitance on both channels and simultaneously checks if any of the two buttons are pressed or released. The two horizontal bars show how much pressure is applied on the two buttons on the pmod. CH1 has 2pF input range and CH2 has 4pF input range. |
{{ : | {{ : |