This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5628 [06 Jul 2012 17:10] – Added the PIC32 driver. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5628 [19 Jul 2012 09:52] – minor changes Dragos Bogdan | ||
---|---|---|---|
Line 21: | Line 21: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 51: | Line 52: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 174: | Line 176: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: | ||
+ | |||
+ | ====== Digilent Cerebot MC7 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD5628 demonstration project on a Digilent Cerebot MC7 platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * PmodDA4 | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDA4 has to be connected to the JB connector of Cerebot MC7 development board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | Following commands were implemented in this version of AD5628 reference project for Cerebot MC7 board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | help? | Displays all available commands. | | ||
+ | | mode= | Selects a mode of operation for the current channel. Accepted values: 0 – 3. | | ||
+ | | mode? | Displays the selected mode of operation for the current channel. | | ||
+ | | channel= | Selects the channel that will be affected by the other commands. Accepted values: 0 – 7 (one channel) or 15 (all channels). | | ||
+ | | channel? | Displays the selected channel. | | ||
+ | | voltage= | Sets the output voltage for the current voltage. Accepted values: 0 – 2.5 (volts). | | ||
+ | | voltage? | Displays the output voltage of the current voltage. | | ||
+ | | register= | Writes the value into the Input Register of the current channel. Accepted values: 0 – 4095. | | ||
+ | | register? | Displays the value written in the Input Register of the current channel. | | ||
+ | |||
+ | Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A. | ||
+ | |||
+ | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page>: | ||
+ | |||
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |