This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5541a [11 Jul 2012 09:11] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5541a [24 Jul 2012 09:38] – Added Arduino driver. Dragos Bogdan | ||
---|---|---|---|
Line 24: | Line 24: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
- | * | + | * [[http:// |
===== Driver Description ===== | ===== Driver Description ===== | ||
The driver contains two parts: | The driver contains two parts: | ||
Line 52: | Line 53: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 164: | Line 166: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: | ||
+ | |||
+ | ====== Digilent Cerebot MC7 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD5541A demonstration project on a Digilent Cerebot MC7 platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * PmodDA3 | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDA3 has to be connected to the JB connector of Cerebot MC7 development board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | Following commands were implemented in this version of AD5541A reference project for Cerebot MC7 board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | help? | Displays all available commands. | | ||
+ | | voltage= | Sets the DAC output voltage. Accepted values: 0 - 2.5 | | ||
+ | | voltage? | Displays last written value. | | ||
+ | | register= | Writes to the DAC register. Accepted values: 0 - 65535. | | ||
+ | | register? | Displays last written value. | | ||
+ | |||
+ | Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A. | ||
+ | |||
+ | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page>: | ||
+ | |||
+ | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino ====== | ||
+ | This section contains a description of the steps required to run the AD5541A Arduino demonstration project on a Digilent Cerebot MX3cK platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * PmodDA3 | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[https:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDA3 has to be connected to the JE connector of Cerebot MX3cK development board. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | Following commands were implemented in this version of AD5541A Arduino reference project for Cerebot MX3cK board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | help? | Displays all available commands. | | ||
+ | | voltage= | Sets the DAC output voltage. Accepted values: 0 - 2.5 | | ||
+ | | voltage? | Displays last written value. | | ||
+ | | register= | Writes to the DAC register. Accepted values: 0 - 65535. | | ||
+ | | register? | Displays last written value. | | ||
+ | |||
+ | Commands can be executed using the serial monitor. | ||
+ | |||
+ | // | ||
+ | |||
+ | The following image shows a list of commands in the serial monitor. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page>: | ||
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |