This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5160 [10 Jul 2012 15:19] – Added driver for PIC32. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5160 [24 Jan 2021 18:25] – Fix bad links Dragos Bogdan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD5160 - Microcontroller | + | ====== AD5160 - No-OS Driver |
- | + | {{page>: | |
- | ===== Supported Devices ===== | + | |
- | * [[adi> | + | |
- | + | ||
- | ===== Evaluation Boards ===== | + | |
- | * PmodDPOT | + | |
- | + | ||
- | ===== Overview ===== | + | |
- | + | ||
- | The [[adi> | + | |
- | + | ||
- | The wiper settings are controllable through an SPI-compatible digital interface. The resistance between the wiper and either end point of the fixed resistor varies linearly with respect to the digital code transferred into the RDAC latch. | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms. | + | |
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
- | * [[http:// | + | |
- | ===== Driver Description | + | ===== Downloads |
- | The driver contains two parts: | + | |
- | * The driver for the AD5160 part, which may be used, without modifications, | + | |
- | * The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements the communication with the device and hides the actual details of the communication protocol to the ADI driver. | + | |
- | The Communication Driver has a standard interface, so the AD5160 driver can be used exactly as it is provided. | + | < |
- | + | * {{: | |
- | There are three functions which are called by the AD5160 driver: | + | |
- | * SPI_Init() – initializes the communication peripheral. | + | |
- | * SPI_Write() – writes data to the device. | + | |
- | * SPI_Read() – reads data from the device. | + | |
- | + | ||
- | {{ : | + | |
- | < | + | |
- | SPI driver architecture | + | |
- | </ | + | |
- | + | ||
- | The following functions are implemented in this version of AD5160 driver: | + | |
- | ^ Function | + | |
- | | unsigned char AD5160_Init(void) | Initializes the SPI communication peripheral. | | + | |
- | | void AD5160_Set(unsigned char value) | Writes data to AD5160. | | + | |
- | + | ||
- | ===== Downloads ===== | + | |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
- | * {{:resources:tools-software:uc-drivers:microchip:ad5160_pic32.zip|AD5160 PIC32 Driver}} | + | * **AD5160 Driver: ** https:// |
+ | * **PmodDPOT Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: ** https://github.com/ | ||
+ | </ | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 54: | Line 21: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
- | * PmodDPOT | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A PmodDPOT has to be connected to the PMOD1 connector. | + | A PmodDPOT has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). |
{{ : | {{ : | ||
- | ==== Software Setup ==== | + | ==== Reference Project Overview |
- | With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured: | + | The reference project: |
+ | * sends to the PmodDPOT an 8 bit value every 2 seconds; | ||
+ | | ||
- | === CSI10 (Clocked Serial Interface 10) – For the AD5541A part and the ST7579 LCD === | + | {{ :resources:tools-software:uc-drivers:renesas:pmod_dpot_rl78g13_screen.jpg? |}} |
- | Choose to generate the Transmit/ | + | |
- | * Transfer mode setting: //**Single transfer mode**// | + | |
- | * Data length setting | + | |
- | * Transfer direction setting: // | + | |
- | * Specification of data timing: //**Type 1**// | + | |
- | * Transfer rate setting – Clock mode: // | + | |
- | * Transfer rate setting – Baudrate: // | + | |
- | * Interrupt setting – Transfer interrupt priority (INTCSI10): // | + | |
- | * Uncheck the callback functions. | + | |
- | === TM00 (Timer 00) – For the DelayMs() function | + | ==== Software Project Tutorial ==== |
- | Configure TM00 as an interval timer: | + | {{page> |
- | * Interval timer setting - Interval value(16 bits): //**1**// ms | + | |
- | * Interval timer setting - Uncheck //Generates INTM00 when counting is started// | + | |
- | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | + | |
- | === Watchdog Timer === | + | |
- | Disable | + | ====== Renesas RL78G14 Quick Start Guide ====== |
- | * Choose | + | This section contains a description of the steps required to run the AD5160 demonstration project on a Renesas RL78G14 platform using the PmodDPOT. |
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[https:// | ||
+ | * [[http://www.digilentinc.com/ | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | | ||
+ | | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD5160 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD5160 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </WRAP> | ||
+ | ==== Hardware Setup ==== | ||
+ | A PmodDPOT has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). | ||
+ | |||
+ | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project sends to the PmodDPOT an 8 bit value every 2 seconds. The sent value and the resistance are displayed on the LCD. | + | The reference project: |
+ | * sends to the PmodDPOT an 8 bit value every 2 seconds; | ||
+ | * the sent value and the resistance are displayed on the LCD. | ||
- | {{ : | + | |
+ | {{ : | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
- | {{page>rl78g13_software_tutorial}} | + | {{page>rl78g14_software_tutorial}} |
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== | ||
Line 102: | Line 80: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
* PmodDPOT | * PmodDPOT | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 127: | Line 105: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
- | |||
- | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
- | This section contains a description of the steps required to run the AD5160 demonstration project on a Digilent Cerebot MX3cK platform. | ||
- | |||
- | ==== Required Hardware ==== | ||
- | * [[http:// | ||
- | * PmodDPOT | ||
- | |||
- | ==== Required Software ==== | ||
- | * [[http:// | ||
- | * [[http:// | ||
- | |||
- | ==== Hardware Setup ==== | ||
- | A PmodDPOT has to be connected to the JE connector of Cerebot MX3cK development board. | ||
- | |||
- | {{ : | ||
- | |||
- | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD5160 reference project for Cerebot MX3cK board. | ||
- | ^ Command ^ Description ^ | ||
- | | help? | Displays all available commands. | | ||
- | | resistance= | Sets the output resistance. Accepted values 0 - 10020. | | ||
- | | resistance? | Displays the last written value. | | ||
- | | register= | Writes to the DAC register of the current channel. Accepted values 0 - 255. | | ||
- | | register? | Displays the last written value. | | ||
- | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | |||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
- | {{ : | ||
- | |||
- | ==== Software Project Setup ==== | ||
- | {{page>: | ||
====== More information ====== | ====== More information ====== | ||
- | {{page> | + | {{page>: |