This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:microchip:adxl362 [09 Oct 2012 09:19] – Replaced Arduino with chipKIT. Dragos Bogdan | resources:tools-software:uc-drivers:microchip:adxl362 [04 Jul 2013 08:57] – [Reference Project Overview] Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **ADXL362 Driver:** https:// | ||
+ | * **PmodACL2 Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers:** https:// | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 17: | Line 20: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodACL2 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The ADXL362 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADXL362 demonstration project for PIC32MX320F128H consists of three parts: the **ADXL362 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 29: | Line 39: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | id? | Device | + | | id? | Displays device |
- | | measure= | Start/stop the measure | + | | measure= | Start/stop the measurement |
- | | temp? | Read the temperature. | | + | | temperature? | Displays |
- | | reset= | Reset the device. | | + | | reset! | Resets |
- | | acceleration? | + | | acceleration? |
+ | | accelerationX? | ||
+ | | accelerationY? | ||
+ | | accelerationZ? | ||
| activity? | Displays the activity status of the device. It runs for 5 motion detections. | | | activity? | Displays the activity status of the device. It runs for 5 motion detections. | | ||
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||