This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:adt7420 [26 Jun 2013 17:16] – source code change and source code put on github Lucian Sin | resources:tools-software:uc-drivers:microchip:adt7420 [22 Jul 2019 14:32] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 10: | Line 10: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
* {{: | * {{: | ||
- | * **ADT7420 Driver: | + | * **ADT7420 Driver: |
- | * **PmodTMP2 Demo for Cerebot MX3cK: ** https:// | + | * **PmodTMP2 Demo for PIC32MX320F128H: ** https:// |
- | * **Cerebot MX3cK Common Drivers: | + | * **PIC32MX320F128H |
</ | </ | ||
- | |||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
This section contains a description of the steps required to run the ADT7420 demonstration project on a Digilent Cerebot MX3cK platform. | This section contains a description of the steps required to run the ADT7420 demonstration project on a Digilent Cerebot MX3cK platform. | ||
Line 25: | Line 24: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
- | * The ADT7420 demonstration project for Digilent Cerebot MX3cK platform. | + | * The ADT7420 demonstration project for PIC32MX320F128H. |
<WRAP round info 80%> | <WRAP round info 80%> | ||
- | The ADT7420 demonstration project for the Digilent Cerebot MX3cK platform | + | The ADT7420 demonstration project for PIC32MX320F128H |
All three parts have to be downloaded. | All three parts have to be downloaded. | ||
</ | </ | ||
- | |||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
A PmodTMP2 has to be connected to the J2 connector of Cerebot MX3cK development board. | A PmodTMP2 has to be connected to the J2 connector of Cerebot MX3cK development board. | ||
Line 43: | Line 41: | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
| reset! | Resets the ADT7420. | | | reset! | Resets the ADT7420. | | ||
- | | mode= | Sets the operational mode for ADT7420. Accepted values: 0 - 3 | | + | | mode= | Sets the operational mode for ADT7420. Accepted values:\\ 0 - Continuos conversions.\\ 1 - One shot.\\ 2 - 1 SPS mode.\\ |
| mode? | Displays the selected operational mode. | | | mode? | Displays the selected operational mode. | | ||
- | | resolution= | Sets the resolution for ADT7420. Accepted values: 0 - 1 | | + | | resolution= | Sets the resolution for ADT7420. Accepted values:\\ 0 - 13 bits resolution.\\ |
| resolution? | Displays the selected resolution. | | | resolution? | Displays the selected resolution. | | ||
| temperature? | | temperature? | ||
Line 53: | Line 51: | ||
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | ||
{{ : | {{ : | ||
- | |||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: |