This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:microchip:adt7420 [26 Jun 2013 17:16] – source code change and source code put on github Lucian Sin | resources:tools-software:uc-drivers:microchip:adt7420 [27 Jun 2013 10:56] – [Required Software] Lucian Sin | ||
---|---|---|---|
Line 11: | Line 11: | ||
* {{: | * {{: | ||
* **ADT7420 Driver: | * **ADT7420 Driver: | ||
- | * **PmodTMP2 Demo for Cerebot MX3cK: ** https:// | + | * **PmodTMP2 Demo for PIC32MX320F128H: ** https:// |
- | * **Cerebot MX3cK Common Drivers: | + | * **PIC32MX320F128H |
</ | </ | ||
- | |||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
This section contains a description of the steps required to run the ADT7420 demonstration project on a Digilent Cerebot MX3cK platform. | This section contains a description of the steps required to run the ADT7420 demonstration project on a Digilent Cerebot MX3cK platform. | ||
Line 25: | Line 24: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
- | * The ADT7420 demonstration project for Digilent Cerebot MX3cK platform. | + | * The ADT7420 demonstration project for PIC32MX320F128H. |
<WRAP round info 80%> | <WRAP round info 80%> | ||
- | The ADT7420 demonstration project for the Digilent Cerebot MX3cK platform | + | The ADT7420 demonstration project for PIC32MX320F128H |
All three parts have to be downloaded. | All three parts have to be downloaded. | ||
</ | </ | ||
- | |||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
A PmodTMP2 has to be connected to the J2 connector of Cerebot MX3cK development board. | A PmodTMP2 has to be connected to the J2 connector of Cerebot MX3cK development board. |