This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:adp5589 [27 Jun 2013 13:23] – [Hardware Setup] Lucian Sin | resources:tools-software:uc-drivers:microchip:adp5589 [22 Jul 2019 14:18] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 9: | Line 9: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
* {{: | * {{: | ||
- | * **ADP5589 Driver: | + | * **ADP5589 Driver: |
* **PmodIOXP Demo for PIC32MX320F128H: | * **PmodIOXP Demo for PIC32MX320F128H: | ||
* **PIC32MX320F128H Common Drivers: | * **PIC32MX320F128H Common Drivers: | ||
Line 41: | Line 41: | ||
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | pwmOnTime= | On time of the PWM pulse. Accepted values: | + | | pwmOnTime= | On time of the PWM pulse. Accepted values:\\ 1 .. 65535[us] - time when the signal is high. | |
- | | pwmOffTime= | Off time of the PWM pulse. Accepted values: | + | | pwmOffTime= | Off time of the PWM pulse. Accepted values:\\ 1 .. 65535[us] - time when the signal is low. | |
| keyPressed? | Displays the last key which was pressed. | | | keyPressed? | Displays the last key which was pressed. | | ||
| keyReleased? | | keyReleased? | ||
Line 49: | Line 49: | ||
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | ||
{{ : | {{ : | ||
- | |||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: |