The AD7980 is a 16-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power, high speed, 16-bit sampling ADC and a versatile serial interface port. On the CNV rising edge, it samples an analog input IN+ between 0 V to REF with respect to a ground sense IN−. The reference voltage, REF, is applied externally and can be set independent of the supply voltage, VDD. Its power scales linearly with throughput.
The SPI-compatible serial interface also features the ability, using the SDI input, to daisy-chain several ADCs on a single, 3-wire bus and provides an optional busy indicator. It is compatible with 1.8 V, 2.5 V, 3 V, or 5 V logic, using the separate supply VIO.
The AD7980 is housed in a 10-lead MSOP or a 10-lead QFN (LFCSP) with operation specified from −40°C to +125°C.
The AD7980-EP supports defense and aerospace applications (AQEC)
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms.
The driver contains two parts:
The Communication Driver has a standard interface, so the AD7980 driver can be used exactly as it is provided.
There are three functions which are called by the AD7980 driver:
SPI driver architecture
The following functions are implemented in this version of AD7980 driver:
Function | Description |
---|---|
char AD7980_Init(void) | Initializes the communication peripheral. |
unsigned short AD7980_Conversion(void) | Initiates conversion and reads data. |
float AD7980_ConvertToVolts(unsigned short rawSample, float vRef) | Converts a 16-bit raw sample to volts. |
This version of AD7980 driver uses the CS Mode 4-Wire, without Busy Indicator mode; the device has to be connected to an SPI-compatible digital host as following:
Signals generated by the driver on the SPI port
HW Platform(s):
This section contains a description of the steps required to run the AD7980 demonstration project on a Digilent Cerebot MX3cK platform.
The AD7980 demonstration project for PIC32MX320F128H consists of three parts: the AD7980 Driver, the EVAL-AD7980-PMDZ Demo for PIC32MX320F128H and the PIC32MX320F128H Common Drivers.
All three parts have to be downloaded.
A has to be connected to the JE connector of Cerebot MX3cK development board.
The following commands were implemented in this version of AD7980 reference project for Cerebot MX3cK board.
Command | Description |
---|---|
help? | Displays all available commands. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the data register in decimal format. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H.
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7980 demonstration project on a Digilent Cerebot MC7 platform.
A EVAL-AD7980-PMDZ has to be connected to the JB connector of Cerebot MC7 development board.
Following commands were implemented in this version of AD7980 reference project for Cerebot MC7 board.
Command | Description |
---|---|
help? | Displays all available commands. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the data register in decimal format. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A.
The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MC7 development board for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7980 chipKIT demonstration project on a Digilent Cerebot MX3cK platform.
A EVAL-AD7980-PMDZ has to be connected to the JE connector of Cerebot MX3cK development board.
Following commands were implemented in this version of AD7980 chipKIT reference project for Cerebot MX3cK board.
Command | Description |
---|---|
help? | Displays all available commands. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the raw data in decimal format. |
Commands can be executed using the serial monitor.
Carriage return has to be selected as a line ending character. The required baud rate is 9600 baud.
The following image shows a list of commands in the serial monitor.
This section presents the steps for developing a chipKIT application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.