This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:ad7303 [01 Oct 2012 15:53] – created Dragos Bogdan | resources:tools-software:uc-drivers:microchip:ad7303 [22 Jul 2019 13:52] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
- | * {{: | + | * {{: |
+ | * **AD7303 Driver: | ||
+ | * **PmodDA1 Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers: | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 22: | Line 25: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The AD7303 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD7303 demonstration project for PIC32MX320F128H consists of three parts: the **AD7303 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 29: | Line 39: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | power= | Powers off/on the current | + | | power= | Powers off/on the selected |
- | | power? | Displays the power status. | | + | | power? | Displays the power status |
- | | channel= | Selects a channel. Accepted values: 0, 1. | | + | | voltage= | Sets the output voltage of the selected |
- | | channel? | Displays the current | + | | voltage? | Displays last written |
- | | voltage= | Sets the output voltage of the current | + | | register= | Writes to the DAC register of the selected |
- | | voltage? | Displays last written value. | | + | | register? | Displays last written value in the DAC register for selected channel. Accepted values:\\ 0 - Select channel A1.\\ 1 - Select channel B1. | |
- | | register= | Writes to the DAC register of the current | + | |
- | | register? | Displays last written value. | | + | |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
Line 86: | Line 94: | ||
{{page>: | {{page>: | ||
- | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino | + | ====== Digilent Cerebot MX3cK Quick Start Guide - chipKIT Project |
- | This section contains a description of the steps required to run the AD7303 | + | This section contains a description of the steps required to run the AD7303 |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
Line 102: | Line 110: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of AD7303 | + | Following commands were implemented in this version of AD7303 |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | |