Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:uc-drivers:microchip:ad7303 [01 Oct 2012 15:53] – created Dragos Bogdanresources:tools-software:uc-drivers:microchip:ad7303 [22 Jul 2019 13:52] (current) – Update no-OS driver link Andrei Drimbarean
Line 7: Line 7:
  
 ===== Downloads ===== ===== Downloads =====
-  * {{:resources:tools-software:uc-drivers:ad7303_generic.zip|AD7303 Generic Driver}} +<WRAP round download 80%>
-  * {{:resources:tools-software:uc-drivers:microchip:ad7303_pic32.zip|AD7303 PIC32 Driver}}+
   * {{:resources:tools-software:uc-drivers:microchip:ad7303_dspic33.zip|AD7303 DSPIC33 Driver}}   * {{:resources:tools-software:uc-drivers:microchip:ad7303_dspic33.zip|AD7303 DSPIC33 Driver}}
-  * {{:resources:tools-software:uc-drivers:microchip:ad7303_arduino.zip|AD7303 Arduino Driver}}+  * {{:resources:tools-software:uc-drivers:microchip:ad7303_arduino.zip|AD7303 chipKIT Driver}} 
 +  * **AD7303 Driver:           ** https://github.com/analogdevicesinc/no-OS/tree/master/drivers/dac/ad7303 
 +  * **PmodDA1 Demo for PIC32MX320F128H: ** https://github.com/analogdevicesinc/no-OS/tree/master/Microchip/PIC32MX320F128H/PmodDA1 
 +  * **PIC32MX320F128H Common Drivers:   ** https://github.com/analogdevicesinc/no-OS/tree/master/Microchip/PIC32MX320F128H/Common 
 +</WRAP>
  
 ====== Digilent Cerebot MX3cK Quick Start Guide ====== ====== Digilent Cerebot MX3cK Quick Start Guide ======
Line 22: Line 25:
   * [[http://www.microchip.com/mplabx|MPLAB X Integrated Development Environment]]   * [[http://www.microchip.com/mplabx|MPLAB X Integrated Development Environment]]
   * [[http://www.microchip.com/mplabxc|MPLAB XC32 compiler]]   * [[http://www.microchip.com/mplabxc|MPLAB XC32 compiler]]
 +  * The AD7303 demonstration project for PIC32MX320F128H.
 +
 +<WRAP round info 80%>
 +The AD7303 demonstration project for PIC32MX320F128H consists of three parts: the **AD7303 Driver**,  the **PmodDA1 Demo for PIC32MX320F128H** and the **PIC32MX320F128H Common Drivers**.
 +
 +All three parts have to be downloaded.
 +</WRAP>
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 29: Line 39:
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
-Following commands were implemented in this version of AD7303 reference project for Cerebot MX3cK board.+The following commands were implemented in this version of AD7303 reference project for Cerebot MX3cK board.
 ^ Command ^ Description ^ ^ Command ^ Description ^
 | help? | Displays all available commands. | | help? | Displays all available commands. |
-| power= | Powers off/on the current channel. Accepted values: 01. | +| power= | Powers off/on the selected channel. Accepted values:\\ channel:\\ - Select channel A1.\\ - Select channel B1.\\ power status:\\ 0 - Power off.\\ 1 - Power on. | 
-| power? | Displays the power status. | +| power? | Displays the power status of the selected channel. Accepted values:\\ - Select channel A1.\\ - Select channel B1. | 
-| channel= | Selects a channel. Accepted values: 01. | +| voltage= | Sets the output voltage of the selected channel. Accepted values:\\ channel:\\ 0 - Select channel A1.\\ 1 - Select channel B1.\\ output voltage:\\ 0..3300 - Desired output voltage in milivolts. | 
-| channel? | Displays the current channel. | +| voltage? | Displays last written voltage value to the DAC for selected channel. Accepted values:\\  0 - Select channel A1.\\ 1 - Select channel B1. | 
-| voltage= | Sets the output voltage of the current channel. Accepted values: 0->3.+| register= | Writes to the DAC register of the selected channel. Accepted values:\\ 0 - Select channel A1.\\ 1 - Select channel B1.\\ register value:\\ 0..255 - Value written to the DAC. | 
-| voltage? | Displays last written value. | +| register? | Displays last written value in the DAC register for selected channel. Accepted values:\\ 0 - Select channel A1.\\ 1 - Select channel B1. |
-| register= | Writes to the DAC register of the current channel. Accepted values: 0 - 255. | +
-| register? | Displays last written value. |+
  
 Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H.
  
-The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral.+The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral.
 {{ :resources:tools-software:uc-drivers:microchip:terminal_pic32.png? |}} {{ :resources:tools-software:uc-drivers:microchip:terminal_pic32.png? |}}
  
Line 86: Line 94:
 {{page>:resources:tools-software:uc-drivers:microchip:dspic33_software_design}} {{page>:resources:tools-software:uc-drivers:microchip:dspic33_software_design}}
  
-====== Digilent Cerebot MX3cK Quick Start Guide - Arduino ====== +====== Digilent Cerebot MX3cK Quick Start Guide - chipKIT Project ====== 
-This section contains a description of the steps required to run the AD7303 Arduino demonstration project on a Digilent Cerebot MX3cK platform.+This section contains a description of the steps required to run the AD7303 chipKIT demonstration project on a Digilent Cerebot MX3cK platform.
  
 ==== Required Hardware ==== ==== Required Hardware ====
Line 102: Line 110:
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
-Following commands were implemented in this version of AD7303 Arduino reference project for Cerebot MX3cK board.+Following commands were implemented in this version of AD7303 chipKIT reference project for Cerebot MX3cK board.
 ^ Command ^ Description ^ ^ Command ^ Description ^
 | help? | Displays all available commands. | | help? | Displays all available commands. |
resources/tools-software/uc-drivers/microchip/ad7303.txt · Last modified: 22 Jul 2019 13:52 by Andrei Drimbarean