This is an old revision of the document!
The AD7156 delivers a complete signal processing solution for capacitive sensors, featuring an ultralow power converter with fast response time.
The AD7156 uses an Analog Devices, Inc., capacitance-to-digital converter (CDC) technology, which combines features important for interfacing to real sensors, such as high input sensitivity and high tolerance of both input parasitic ground capacitance and leakage current.
The integrated adaptive threshold algorithm compensates for any variations in the sensor capacitance due to environmental factors like humidity and temperature or due to changes in the dielectric material over time.
By default, the AD7156 operates in standalone mode using the fixed power-up settings and indicates detection on two digital outputs. Alternatively, the AD7156 can be interfaced to a micro-controller via the serial interface, the internal registers can be programmed with user-defined settings, and the data and status can be read from the part.
The AD7156 operates with a 1.8 V to 3.6 V power supply. It is specified over the temperature range of −40°C to +85°C.
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms.
The driver contains two parts:
There are three functions which are called by the AD7156 driver:
I2C driver architecture
The following functions are implemented in this version of AD7156 driver:
Function | Description |
---|---|
void AD7156_GetRegisterValue(unsigned char* pReadData, unsigned char registerAddress, unsigned char bytesNumber) | Performs a burst read of a specified number of registers. |
void AD7156_SetRegisterValue(unsigned short registerValue, unsigned char registerAddress, unsigned char bytesNumber) | Writes data into one or two registers. |
char AD7156_Init(void) | Initializes the communication peripheral and checks if the device is present. |
void AD7156_Reset(void) | Resets the device. |
void AD7156_SetPowerMode(unsigned char pwrMode) | Sets the converter mode of operation. |
void AD7156_ChannelState(unsigned char channel, unsigned char enableConv) | Enables or disables conversion on the selected channel. |
void AD7156_SetRange(unsigned channel, unsigned char range) | Sets the input range of the specified channel. |
float AD7156_GetRange(unsigned channel) | Reads the range bits from the device and returns the range in pF. |
void AD7156_SetThresholdMode(unsigned char thrMode, unsigned char thrFixed) | Selects the threshold mode of operation. |
void AD7156_SetThreshold(unsigned char channel, float pFthr) | Writes to the threshold register when threshold fixed mode is enabled. |
void AD7156_SetSensitivity(unsigned char channel, float pFsensitivity) | Writes a value(pF) to the sensitivity register. This functions should be used when adaptive threshold mode is selected. |
unsigned short AD7156_ReadChannelData(unsigned char channel) | Reads a 12-bit sample from the selected channel. |
unsigned short AD7156_WaitReadChannelData(unsigned char channel) | Waits for a finished CDC conversion and reads a 12-bit sample from the selected channel. |
float AD7156_ReadChannelCapacitance(unsigned char channel) | Reads a sample the selected channel and converts the data to picofarads(pF). |
float AD7156_WaitReadChannelCapacitance(unsigned char channel) | Waits for a finished CDC conversion the selected channel, reads a sample and converts the data to picofarads(pF). |
HW Platform(s):
This section contains a description of the steps required to run the AD7156 demonstration project on a Digilent Cerebot MX3cK platform.
The following commands were implemented in this version of AD7156 reference project for Cerebot MX3cK board.
Command | Description |
---|---|
help? | Displays all available commands. |
channelRange? | Displays the set range for the selected channel. Accepted values: 1 - Displays the channel 1's range. 2 - Displays the channel 2's range. |
channelRange= | Selects the range of the selected channel. Accepted values: channel: 1 - Select channel 1. 2 - Select channel 2. range: 0 - 0..2pF. 1 - 0..0.5pF 2 - 0..1pF 3 - 0..4pF. |
powerMode? | Displays the current power mode. |
powerMode= | Selects the power mode of the device. Accepted values: 0 - Idle. 1 - Continuous conversions. 2 - Single conversion. 3 - Power-down. |
channelEnable= | Enables or disabled conversions on selected channel. Accepted values: channel: 1 - Select channel 1. 2 - Select channel 2. enable: 0 - Disable conversions on selected channel. 1 - Enable conversions on selected channel. |
samples? | Reads 50 samples form the enabled channels and displays the data in pF. |
buttons? | Checks if any of the two buttons are pressed or released. |
reset! | Resets the device. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H.
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7156 demonstration project on a Digilent Cerebot MC7 platform.
Following commands were implemented in this version of AD7156 reference project for Cerebot MC7 board.
Command | Description |
---|---|
help? | Displays all available commands. |
range= | Selects the range of the channels. Accepted values: 0-3. |
power= | Selects the power mode of the device. Accepted values: 0 - 3. |
channel1= | Enables or disabled conversions on channel 1. Accepted values 0-1. |
channel2= | Enables or disabled conversions on channel 2. Accepted values 0-1. |
samples? | Reads 50 samples form the enabled channels and displays the data as pF. |
buttons? | Checks if any of the two buttons are pressed or released. |
reset= | Resets the device. Accepted value: 1. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A.
The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MC7 development board for controlling and monitoring the operation of the ADI part.