This is an old revision of the document!
The AD7091R is a 12-bit successive approximation analog-to-digital converter (ADC) that offers ultralow power consumption (typically 349 µA at 3 V and 1 MSPS) while achieving fast throughput rates (1 MSPS with a 50 MHz SCLK). The AD7091R uses advanced design and process techniques to achieve this very low power dissipation at high throughput rates. The part also features an on-chip, accurate 2.5 V reference.
Operating from a single 2.7 V to 5.25 V power supply, the part contains a wide bandwidth track-and-hold amplifier that can handle input frequencies in excess of 7 MHz. The AD7091R also features an on-chip conversion clock and high speed serial interface. The conversion process and data acquisition are controlled using a CONVST signal and an internal oscillator.
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms.
The driver contains two parts:
The Communication Driver has a standard interface, so the AD7091R driver can be used exactly as it is provided.
There are three functions which are called by the AD7091R driver:
SPI driver architecture
The following functions are implemented in this version of AD7091R driver:
Function | Description |
---|---|
char AD7091R_Init(void) | Initializes the SPI communication peripheral. |
void AD7091R_SoftwareReset(void) | Initiate a software reset of the device. |
unsigned short AD7091R_ReadSample(void) | Initiates one conversion and reads back the result. |
void AD7091R_PowerDown(void) | Puts the device in power-down mode. |
void AD7091R_PowerUp(void) | Powers up the device. |
float AD7091R_ConvertToVolts(short rawSample, float vRef) | Converts a 12-bit raw sample to volts. |
HW Platform(s):
This section contains a description of the steps required to run the AD7091R demonstration project on a Digilent Cerebot MX3cK platform.
The AD7091R demonstration project for PIC32MX320F128H consists of three parts: the AD7091R Driver, the PmodAD6 Demo for PIC32MX320F128H and the PIC32MX320F128H Common Drivers.
All three parts have to be downloaded.
A PmodAD6 has to be connected to the JE connector of Cerebot MX3cK development board.
The following commands were implemented in this version of AD7091R reference project for Cerebot MX3cK board.
Command | Description |
---|---|
help? | Displays all available commands. |
reset= | Initiates a software reset. |
power? | Displays the power status of the device. |
power= | Powers on/off the device. Accepted values: 0 - Power off. 1 - Power on. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the value from the register. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H.
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7091R demonstration project on a Digilent Cerebot MC7 platform.
Following commands were implemented in this version of AD7091R reference project for Cerebot MC7 board.
Command | Description |
---|---|
help? | Displays all available commands. |
reset= | Initiates a software reset. Accepted value: 1. |
power= | Powers up or down the device. Accepted values: 0 - 1. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the raw data in decimal format. |
Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A.
The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral.
This section presents the steps for developing a software application that will run on the Digilent Cerebot MC7 development board for controlling and monitoring the operation of the ADI part.
This section contains a description of the steps required to run the AD7091R chipKIT demonstration project on a Digilent Cerebot MX3cK platform.
Following commands were implemented in this version of AD7091R chipKIT reference project for Cerebot MX3cK board.
Command | Description |
---|---|
help? | Displays all available commands. |
reset= | Initiates a software reset. Accepted value: 1. |
power= | Powers up or down the device. Accepted values: 0 - 1. |
voltage? | Initiates a conversion and displays the captured voltage. |
register? | Initiates a conversion and displays the raw data in decimal format. |
Commands can be executed using the serial monitor.
Carriage return has to be selected as a line ending character. The required baud rate is 9600 baud.
The following image shows a list of commands in the serial monitor.
This section presents the steps for developing a chipKIT application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.