The MAX31865 is an easy-to-use resistance-to-digital converter optimized for platinum resistance temperature detectors (RTDs). An external resistor sets the sensitivity for the RTD being used and a precision delta-sigma ADC converts the ratio of the RTD resistance to the reference resistance into digital form.
The MAX31865’s inputs are protected against overvoltage faults as large as Q45V. Programmable detection of RTD and cable open and short conditions is included.
The goal of ADI Microcontroller No-OS is to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, and to help those customers using microcontrollers with ADI parts. ADI No-OS offers generic drivers, which can be used as a base for any microcontroller platform and also example projects, which are using these drivers on various microcontroller platforms.
For more information about ADI No-OS and supported microcontroller platforms, visit the No-OS User Guide.
The source code for MAX31865 driver can be found here:
This driver also uses the ADI utility library, so make sure you also add the necessary files to your project. The source code for the util library can be found here:
To use the MAX32865 No-OS Driver, you need to provide the specific implementation for the communication APIs and the specific types they use. If the SPI communication is chosen, there are three functions which are called by the MAX31865 driver and have to be implemented:
no_os_spi_init() | initializes the communication peripheral. |
no_os_spi_write_and_read() | writes and reads data to/from the device. |
no_os_spi_remove() | deinitializes the communication peripheral. |
And there are two data types that have to be defined:
no_os_spi_desc | structure holding the SPI descriptor |
no_os_spi_init_param | structure holding the parameters for SPI initialization |
An example of a header file containing the prototypes of the functions which have to be implemented, along with some generic data types they are using, can be found below:
Source code documentation for the driver is automatically generated using the Doxygen tool and can be accessed in these links:
To use the device, you need to provide the support for the communication protocol (SPI) as mentioned above.
The first API function to be called is max31865_init. Make sure that it returns 0. This indicates a successful driver initialization.
When no conversions are being performed, VBIAS may be disabled to reduce power dissipation. When automatic (continuous) conversion mode is selected, VBIAS remains on continuously.
max31865_enable_bias | Enable or disables the bias voltage on the RTD sensor |
Conversion mode is configurable between automatic conversion mode where continuous conversion is used and “Normally Off” mode where 1-shot conversion is used, this also has a selectable 50/60Hz conversion rates.
max31865_auto_convert | Option for continuous conversions between 50/60 Hz |
max31865_enable_50Hz | Option for 50Hz or 60Hz noise filters |
The High Fault Threshold and Low Fault Threshold registers select the trip thresholds for RTD fault detection. The results of RTD conversions are compared with the values in these registers to generate the “Fault” bits in the Fault Status register. The RTD Data Registers, High Fault Threshold Registers, and Low Fault Threshold Registers all have the same format.
max31865_set_threshold | Update the contents of the HIGH and LOW FAULT registers of max31865 |
max31865_get_lower_threshold | Read the raw 16-bit lower threshold value |
max31865_get_upper_threshold | Read the raw 16-bit upper threshold value |
MAX31865 can be configured to support 2-wire, 3-wire and 4-wire types of RTD sensors.
max31865_set_wires | N-wire option for RTD measurement setup |
int ret; uint16_t low_thres, high_thres, rtd_raw; struct max_spi_init_param max31865_extra = { .num_slaves = 1, .polarity = SPI_SS_POL_LOW, .vssel = MXC_GPIO_VSSEL_VDDIOH, }; struct max31865_init_param max31865_ip = { .spi_init.device_id = 1, .spi_init.max_speed_hz = 2000000, .spi_init.chip_select = 0, .spi_init.mode = NO_OS_SPI_MODE_3, .spi_init.bit_order = NO_OS_SPI_BIT_ORDER_MSB_FIRST, .spi_init.platform_ops = &max_spi_ops, .spi_init.extra = &max31865_extra, }; struct max31865_dev *max31865_device; ret = max31865_init(&max31865_device, &max31865_ip); if (ret) return ret; /* Set upper and lower threshold values */ ret = max31865_set_threshold(max31865_device, 0x2121, 0x4114); if (ret) return ret; /* Obtain lower threshold value */ ret = max31865_get_lower_threshold(max31865_device, &low_thres); if (ret) return ret; /* Obtain upper threshold value*/ ret = max31865_get_upper_threshold(max31865_device, &high_thres); if(ret) return ret; /* Enable 50Hz filter */ ret = max31865_enable_50Hz(max31865_device, true); if (ret) return ret; /* Configure for even wire setting */ ret = max31865_set_wires(max31865_device, false); if (ret) return ret; while(1){ /* Read rtd register raw value (16 bits) */ ret = max31865_read_rtd(max31865_device, &rtd_raw); if (ret) return ret; MXC_Delay(5000); }// end while max31865_remove(max31865_device); return 0;