This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:uc-drivers:hmc7044 [07 Feb 2020 09:27] – example Darius B | resources:tools-software:uc-drivers:hmc7044 [07 Feb 2020 12:15] (current) – doxygen Darius B | ||
---|---|---|---|
Line 30: | Line 30: | ||
[[https:// | [[https:// | ||
+ | ===== Source Code Documentation ===== | ||
+ | [[http:// | ||
+ | |||
+ | [[http:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
The driver implements the necessary routines for managing the device and communicates with the device over an SPI interface. The SPI communication layer is not implemented by the driver and has to be provided by the user at the driver initialization phase. | The driver implements the necessary routines for managing the device and communicates with the device over an SPI interface. The SPI communication layer is not implemented by the driver and has to be provided by the user at the driver initialization phase. |