This is an old revision of the document!
The ADXL372 is an ultralow power, 3-axis, ±200 g MEMS accelerometer that consumes 22 μA at a 3200 Hz output data rate (ODR). The ADXL372does not power cycle its front end to achieve its low power operation and therefore does not run the risk of aliasing the output of the sensor.
The ADXL372 provides 12-bit output data at 100 mg/LSB scale factor. The user can access configuration and data registers via the serial peripheral interface (SPI) or limited I2C protocol. The ADXL372 operates over a wide supply voltage range and is available in a 3 mm × 3.25 mm × 1.06 mm package.
In addition to its ultralow power consumption, the ADXL372 has many features to enable impact detection while providing system level power reduction. The device includes a deep multimode output first in, first out (FIFO), several activity detection modes, and a method for capturing only the peak acceleration of over threshold events.
The ADXL372 operates on a wide 1.6 V to 3.5 V supply range. ADXL372 is available in a 3 mm × 3.25 mm × 1.06 mm package.
Function | Description |
---|---|
int32_t adxl372_init(adxl372_dev **device, adxl372_init_param init_param) | Initialize the device. |
int32_t adxl372_get_accel_data(adxl372_dev *dev, adxl372_xyz_accel_data *accel_data) | Retrieve 3-axis acceleration data. |
int32_t adxl372_get_highest_peak_data(adxl372_dev *dev, adxl372_xyz_accel_data *max_peak) | Retrieve the highest magnitude (x, y, z) sample recorded since the last read of the MAXPEAK registers. |
int32_t adxl372_get_fifo_xyz_data(adxl372_dev *dev, adxl372_xyz_accel_data *samples, uint16_t cnt) | Get the data stored in FIFO. |
int32_t adxl_service_fifo_ev(adxl372_dev *dev, adxl372_xyz_accel_data *fifo_data, uint16_t *fifo_entries) | Retrieve data stored in FIFO. Can be used in polling mode, but works best when interrupts are used. |
int32_t adxl372_configure_fifo(adxl372_dev *dev, adxl372_fifo_mode mode, adxl372_fifo_format format, uint16_t fifo_samples) | Configure the operating parameters for the FIFO. |
int32_t adxl372_reset(adxl372_dev *dev) | Software reset. |
int32_t adxl372_get_status(adxl372_dev *dev, uint8_t *status1, uint8_t *status2, uint16_t *fifo_entries) | Get the STATUS, STATUS2, FIFO_ENTRIES and FIFO_ENTRIES2 registers data. |
int32_t adxl372_interrupt_config(adxl372_dev *dev, adxl372_irq_config int1, adxl372_irq_config int2) | Configure the INT1 and INT2 interrupt pins. |
int32_t adxl372_set_filter_settle(adxl372_dev *dev, adxl372_filter_settle mode) | Set the filter settling period. |
int32_t adxl372_set_inactivity_time(adxl372_dev *dev, uint16_t time) | Set the inactivity timer. |
int32_t adxl372_set_activity_time(adxl372_dev *dev, uint16_t time) | Set the activity timer. |
int32_t adxl372_set_wakeup_rate(adxl372_dev *dev, adxl372_wakeup_rate wur) | Set the Timer Rate for Wake-Up Mode. |
int32_t adxl372_set_instant_on_th(adxl372_dev *dev, adxl372_instant_on_th_mode mode) | Select instant on threshold. |
int32_t adxl372_set_odr(adxl372_dev *dev, adxl372_odr odr) | Set Output data rate. |
int32_t adxl372_set_act_proc_mode(adxl372_dev *dev, adxl372_act_proc_mode mode) | Link/Loop Activity Processing. |
int32_t adxl372_set_bandwidth(adxl372_dev *dev, adxl372_bandwidth bw) | Select the desired output signal bandwidth. |
int32_t adxl372_set_autosleep(adxl372_dev *dev, bool enable) | Autosleep. When set to 1, autosleep is enabled, and the device enters wake-up mode automatically upon detection of inactivity. |
int32_t adxl372_set_op_mode(adxl372_dev *dev, adxl372_op_mode op_mode) | Set the mode of operation. |
int32_t adxl372_set_activity_threshold(adxl372_dev *dev, adxl372_th_activity act, uint16_t thresh, bool referenced, bool enable) | Set the threshold for activity detection for all 3-axis |
int32_t adxl372_spi_write_mask(adxl372_dev *dev, uint8_t reg_addr, uint32_t mask, uint8_t data) | SPI write to device using a mask. |
int32_t adxl372_spi_reg_write(adxl372_dev *dev, uint8_t reg_addr, uint8_t reg_data) | Write to device. |
int32_t adxl372_spi_reg_read_multiple(adxl372_dev *dev, uint8_t reg_addr, uint8_t *reg_data, uint16_t count) | Multibyte read from device. A register read begins with the address and autoincrements for each aditional byte in the transfer. |
int32_t adxl372_spi_reg_read(adxl372_dev *dev, uint8_t reg_addr, uint8_t *reg_data) | Read from device. |