Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:adxl372 [13 Feb 2018 11:01] Stefan Poparesources:tools-software:uc-drivers:adxl372 [22 Jul 2019 09:57] (current) – Update no-OS driver link Andrei Drimbarean
Line 41: Line 41:
 |<code c>int32_t adxl372_set_activity_time(adxl372_dev *dev, uint16_t time)</code>| Set the activity timer.| |<code c>int32_t adxl372_set_activity_time(adxl372_dev *dev, uint16_t time)</code>| Set the activity timer.|
 |<code c>int32_t adxl372_set_wakeup_rate(adxl372_dev *dev, adxl372_wakeup_rate wur)</code>| Set the Timer Rate for Wake-Up Mode.| |<code c>int32_t adxl372_set_wakeup_rate(adxl372_dev *dev, adxl372_wakeup_rate wur)</code>| Set the Timer Rate for Wake-Up Mode.|
 +|<code c>int32_t adxl372_set_instant_on_th(adxl372_dev *dev, adxl372_instant_on_th_mode mode)</code>| Select instant on threshold.|
 +|<code c>int32_t adxl372_set_odr(adxl372_dev *dev, adxl372_odr odr)</code>| Set Output data rate.|
 +|<code c>int32_t adxl372_set_act_proc_mode(adxl372_dev *dev, adxl372_act_proc_mode mode)</code>| Link/Loop Activity Processing.|
 +|<code c>int32_t adxl372_set_bandwidth(adxl372_dev *dev, adxl372_bandwidth bw)</code>| Select the desired output signal bandwidth.|
 +|<code c>int32_t adxl372_set_autosleep(adxl372_dev *dev, bool enable)</code>| Autosleep. When set to 1, autosleep is enabled, and the device enters wake-up mode automatically upon detection of inactivity.|
 +|<code c>int32_t adxl372_set_op_mode(adxl372_dev *dev, adxl372_op_mode op_mode)</code>| Set the mode of operation.|
 +|<code c>int32_t adxl372_set_activity_threshold(adxl372_dev *dev, adxl372_th_activity act, uint16_t thresh, bool referenced, bool enable)</code>| Set the threshold for activity detection for all 3-axis|
 +|<code c>int32_t adxl372_spi_write_mask(adxl372_dev *dev, uint8_t reg_addr, uint32_t mask, uint8_t data)</code>| SPI write to device using a mask.|
 +|<code c>int32_t adxl372_spi_reg_write(adxl372_dev *dev, uint8_t reg_addr, uint8_t reg_data)</code>| Write to device.|
 +|<code c>int32_t adxl372_spi_reg_read_multiple(adxl372_dev *dev, uint8_t reg_addr, uint8_t *reg_data, uint16_t count)</code>| Multibyte read from device. A register read begins with the address and autoincrements for each aditional byte in the transfer.|
 +|<code c>int32_t adxl372_spi_reg_read(adxl372_dev *dev, uint8_t reg_addr, uint8_t *reg_data)</code>| Read from device.|
 +
 +==== Types Declarations ====
 +|<code c>
 +typedef enum {
 + ADXL372_X_AXIS,
 + ADXL372_Y_AXIS,
 + ADXL372_Z_AXIS
 +} adxl372_axis;
 +
 +typedef enum {
 + ADXL372_STANDBY,
 + ADXL372_WAKE_UP,
 + ADXL372_INSTANT_ON,
 + ADXL372_FULL_BW_MEASUREMENT
 +} adxl372_op_mode;
 +
 +typedef enum {
 + ADXL372_BW_200HZ,
 + ADXL372_BW_400HZ,
 + ADXL372_BW_800HZ,
 + ADXL372_BW_1600HZ,
 + ADXL372_BW_3200HZ
 +} adxl372_bandwidth;
 +
 +typedef enum {
 + ADXL372_DEFAULT,
 + ADXL372_LINKED,
 + ADXL372_LOOPED
 +} adxl372_act_proc_mode;
 +
 +typedef enum {
 + ADXL372_ODR_400HZ,
 + ADXL372_ODR_800HZ,
 + ADXL372_ODR_1600HZ,
 + ADXL372_ODR_3200HZ,
 + ADXL372_ODR_6400HZ
 +} adxl372_odr;
 +
 +typedef enum {
 + ADXL372_INSTANT_ON_LOW_TH,
 + ADXL372_INSTANT_ON_HIGH_TH
 +} adxl372_instant_on_th_mode;
 +
 +typedef enum {
 + ADXL372_WUR_52ms,
 + ADXL372_WUR_104ms,
 + ADXL372_WUR_208ms,
 + ADXL372_WUR_512ms,
 + ADXL372_WUR_2048ms,
 + ADXL372_WUR_4096ms,
 + ADXL372_WUR_8192ms,
 + ADXL372_WUR_24576ms
 +} adxl372_wakeup_rate;
 +
 +typedef enum {
 + ADXL372_ACTIVITY,
 + ADXL372_ACTIVITY2,
 + ADXL372_INACTIVITY
 +} adxl372_th_activity;
 +
 +typedef enum {
 + ADXL372_FILTER_SETTLE_370,
 + ADXL372_FILTER_SETTLE_16
 +} adxl372_filter_settle;
 +
 +typedef enum {
 + ADXL372_XYZ_FIFO,
 + ADXL372_X_FIFO,
 + ADXL372_Y_FIFO,
 + ADXL372_XY_FIFO,
 + ADXL372_Z_FIFO,
 + ADXL372_XZ_FIFO,
 + ADXL372_YZ_FIFO,
 + ADXL372_XYZ_PEAK_FIFO,
 +} adxl372_fifo_format;
 +
 +typedef enum {
 + ADXL372_FIFO_BYPASSED,
 + ADXL372_FIFO_STREAMED,
 + ADXL372_FIFO_TRIGGERED,
 + ADXL372_FIFO_OLD_SAVED
 +} adxl372_fifo_mode;
 +
 +typedef struct {
 + adxl372_fifo_mode fifo_mode;
 + adxl372_fifo_format fifo_format;
 + uint16_t fifo_samples;
 +} adxl372_fifo_config;
 +
 +typedef struct {
 + uint16_t thresh;
 + bool referenced;
 + bool enable;
 +} adxl372_activity_threshold;
 +
 +typedef struct {
 + uint16_t x;
 + uint16_t y;
 + uint16_t z;
 +} adxl372_xyz_accel_data;
 +
 +typedef struct {
 + bool data_rdy;
 + bool fifo_rdy;
 + bool fifo_full;
 + bool fifo_ovr;
 + bool inactivity;
 + bool activity;
 + bool awake;
 + bool low_operation;
 +} adxl372_irq_config;
 +
 +typedef struct {
 + /* SPI */
 + spi_desc *spi_desc;
 + /* GPIO */
 + gpio_desc *gpio_int1;
 + gpio_desc *gpio_int2;
 + /* Device Settings */
 + adxl372_bandwidth bw;
 + adxl372_odr odr;
 + adxl372_wakeup_rate wur;
 + adxl372_act_proc_mode act_proc_mode;
 + adxl372_instant_on_th_mode th_mode;
 + adxl372_fifo_config fifo_config;
 +} adxl372_dev;
 +
 +typedef struct {
 + /* SPI */
 + spi_init_param spi_init;
 + /* GPIO */
 + int8_t gpio_int1;
 + int8_t gpio_int2;
 + /* Device Settings */
 + adxl372_bandwidth bw;
 + adxl372_odr odr;
 + adxl372_wakeup_rate wur;
 + adxl372_act_proc_mode act_proc_mode;
 + adxl372_instant_on_th_mode th_mode;
 + adxl372_activity_threshold activity_th;
 + adxl372_activity_threshold activity2_th;
 + adxl372_activity_threshold inactivity_th;
 + uint8_t activity_time;
 + uint16_t inactivity_time;
 + adxl372_filter_settle filter_settle;
 + adxl372_fifo_config fifo_config;
 + adxl372_irq_config int1_config;
 + adxl372_irq_config int2_config;
 + adxl372_op_mode op_mode;
 +} adxl372_init_param;
 +</code>|
 +===== No-OS Downloads =====
 +<WRAP round download 50%>
 +  * {{https://github.com/analogdevicesinc/no-OS/tree/master/drivers/accel/adxl372|adxl372 source and header files.}}
 +</WRAP>
resources/tools-software/uc-drivers/adxl372.txt · Last modified: 22 Jul 2019 09:57 by Andrei Drimbarean