This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:adxl355 [22 Mar 2022 14:10] – [ADXL355 Driver] Ramona Bolboaca | resources:tools-software:uc-drivers:adxl355 [27 Jun 2023 10:37] (current) – [ADXL355 IIO Code Driver Documentation] Ramona Bolboaca | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADXL355 Driver ====== | + | ====== ADXL355 |
===== Supported Devices ===== | ===== Supported Devices ===== | ||
Line 26: | Line 26: | ||
The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | ||
- | For more information about ADI No-OS and supported microcontroller platforms see: [[: | + | For more information about ADI No-OS and supported microcontroller platforms see: [[: |
Line 72: | Line 72: | ||
==== ADXL355 Code Driver Documentation ==== | ==== ADXL355 Code Driver Documentation ==== | ||
Source code documentation for the driver is automatically generated using the Doxygen tool and it is available below: | Source code documentation for the driver is automatically generated using the Doxygen tool and it is available below: | ||
- | * [[http:// | + | * [[http:// |
- | * [[http:// | + | * [[http:// |
Line 204: | Line 204: | ||
==== ADXL355 IIO Code Driver Documentation ==== | ==== ADXL355 IIO Code Driver Documentation ==== | ||
Source code documentation for the IIO driver is automatically generated using the Doxygen tool and it is available below: | Source code documentation for the IIO driver is automatically generated using the Doxygen tool and it is available below: | ||
- | * [[http:// | + | * [[http:// |
- | * [[http:// | + | * [[http:// |
==== ADXL355 IIO Device Configuration ==== | ==== ADXL355 IIO Device Configuration ==== | ||
=== Device Attributes === | === Device Attributes === | ||
ADXL355 IIO device does not have any device specific attributes. | ADXL355 IIO device does not have any device specific attributes. | ||
=== Device Channels === | === Device Channels === | ||
- | ADXL355 IIO device has 0 input channels and 4 output | + | ADXL355 IIO device has 0 output |
== Acceleration channels == | == Acceleration channels == | ||
Line 266: | Line 266: | ||
The ADXL355 IIO devices driver supports the usage of a data buffer for reading purposes. | The ADXL355 IIO devices driver supports the usage of a data buffer for reading purposes. | ||
- | === Device triggers === | ||
- | TBD | ||
==== ADXL355 IIO Driver Initialization Example ==== | ==== ADXL355 IIO Driver Initialization Example ==== | ||
< | < |