Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:uc-drivers:adgs5412 [22 Jul 2019 14:22] – Update no-OS driver link Andrei Drimbareanresources:tools-software:uc-drivers:adgs5412 [02 Jun 2020 17:08] (current) – [Supported Devices] Stephen Nugent
Line 10: Line 10:
   * [[adi>ADGS1209]]     * [[adi>ADGS1209]]  
   * [[adi>ADGS1408]]     * [[adi>ADGS1408]]  
-  * [[adi>ADGS1409]]  +  * [[adi>ADGS1409]] 
 +  * [[adi>ADGS1414D]]
 ===== Overview ===== ===== Overview =====
 The [[adi>ADGS5412]] contains four independent single-pole/single-throw (SPST) switches. An SPI interface controls the switches. The SPI interface has robust error detection features. These are CRC error detection, Invalid Read/Write Address detection and SCLK count error detection. The [[adi>ADGS5412]] contains four independent single-pole/single-throw (SPST) switches. An SPI interface controls the switches. The SPI interface has robust error detection features. These are CRC error detection, Invalid Read/Write Address detection and SCLK count error detection.
resources/tools-software/uc-drivers/adgs5412.txt · Last modified: 02 Jun 2020 17:08 by Stephen Nugent