This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:transceiver-toolbox:examples:pluto_lte_app [16 Jul 2020 16:16] – Updated screenshot Srikanth Pagadarai | resources:tools-software:transceiver-toolbox:examples:pluto_lte_app [11 Jan 2021 19:21] – fix link Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
This article describes the MATLAB app that ADI has developed in order to run LTE's eNodeB Test Model waveforms using ADALM-Pluto. Using this app, users connect the transmit and receive ports of their PlutoSDR using a cable and verify that the error vector magnitude (EVM) of the AD9363 transceiver inside their Pluto SDR conforms to the specifications listed in the datasheet. Users can view the EVM corresponding to the channels present in the LTE downlink resource grid over time, frequency and resource grid also. In order to run the code that builds this app, users would need: | This article describes the MATLAB app that ADI has developed in order to run LTE's eNodeB Test Model waveforms using ADALM-Pluto. Using this app, users connect the transmit and receive ports of their PlutoSDR using a cable and verify that the error vector magnitude (EVM) of the AD9363 transceiver inside their Pluto SDR conforms to the specifications listed in the datasheet. Users can view the EVM corresponding to the channels present in the LTE downlink resource grid over time, frequency and resource grid also. In order to run the code that builds this app, users would need: | ||
- | * [[mw> | + | * [[mw> |
* [[mw> | * [[mw> | ||
* [[mw> | * [[mw> | ||
Line 12: | Line 12: | ||
- an ADALM-Pluto | - an ADALM-Pluto | ||
- a loopback cable with SMA male ports on both ends | - a loopback cable with SMA male ports on both ends | ||
+ | During the application installation, | ||
A screenshot of the app in action is shown below. To run the app, users connect a PlutoSDR to their host computer and select the constellation of PDSCH (LTE's physical channel that carries user data), bandwidth, and channel indicated by the LO (MHz) field in the top left panel of the app. Test models are standardized tests defined within [[https:// | A screenshot of the app in action is shown below. To run the app, users connect a PlutoSDR to their host computer and select the constellation of PDSCH (LTE's physical channel that carries user data), bandwidth, and channel indicated by the LO (MHz) field in the top left panel of the app. Test models are standardized tests defined within [[https:// |