This is an old revision of the document!
When Sigma Studio+ is launched and a new project is created, the System tab appears with PC device present. In the System tab, the user must select the appropriate platform for which the project being created is to be targeted and the communication device which is used for communicating to the selected platform must also be chosen. Please check the Supported Platforms page to find all the supported platforms, processors and communication devices. Once the desired platform and communication device is chosen connections have to be established from PC to the communication device and from the communication device to the platform.Few example configurations are shown below for reference.
SC589 Platform connected to USBi communication device
21569 Platform connected to Aardvark communication device