This is an old revision of the document!
Click here to return back
SigmaStudio+ Shortcuts
Keyboard Shortcuts
Make a Copy of Shape
Select the shape to be copied. Click Alt and drag the shape to create a copy of the shape
Select Multiple Shapes
Individually click on the items to select or click on the left mouse button and drag the cursor over relevant items while holding the Ctrl key
Insert Multiple Connections Between Two Shapes
Press Alt while making a connection between an output pin of the first module to an input pin of the second module. The remaining output pins of the first module will get automatically connected to the remaining input pins of the second module in the same order of the pins
Insert Alias Pin
Press Ctrl and Right Click on an output pin using mouse to insert an Alias pin connected to the output pin
Toggle Control Value
Use Ctrl + T to toggle between the current and previous values of the current control
Module Control Shortcuts
Use Spacebar to toggle the value of checkbox control. Use Up/Down keys to change the value of knob, slider and numeric up-down controls
UI Shortcuts
Navigate to the shape from output window
Users can navigate to the shape from the output window if the connector is missing while linking
Collapse tree view items
Users can collapse the tree view items in one click
Navigating from project window
Users can navigate to the module in the schematic by double clicking on that module from the project window
Link Compile Download from project window
Users can do link compile download from the project window as well by selecting the platform