SigmaStudio+ supports manually upgrading the plugin versions through the plugin version management.This is available under Tools as Project version control .When the user selects the plugin version management under project version control ,It will list all the plugins in the current project for which higher versions are available.
The list may include details like the plugin name,current version,available version,version description and update option of the higher version of the plugins if available.
When the user clicks on the upgrade option,the plugins will be updated to the selected version.Only Upgrading of the plugins is supported with the plugin version management,downgrading is not supported.Individual plugins can be downgraded using the properties window.