This section provides different ways of accessing canvas and settings windows in a project.
Following are the different ways of accessing canvas and settings windows in a project:
1. Users can double click on the platform to open its canvas or right click on the platform and open its settings and canvas (refer the image below).
2. Users can open the processor's settings and the canvas from the project window (refer the image below).
3. Users can open the processor's settings and the canvas from the schematic window using the settings and canvas icon (refer the image below).