This is an old revision of the document!
To organize your project visually, it often helps to create an alias to provide a clear connective reference (a “jump”) in the signal flow in the schematic. An Alias consists of a pair of alias input and alias output blocks. Using alias blocks can reduce the visual clutter in the schematic window created by long wire connections.
An alias can be created in two ways:
It is possible to have multiple output alias pins created from the same Alias Input pin.
Right clicking on Input Alias will display the context menu. Use the option 'Add Alias Output' to add output alias. That output Alias can be moved to anywhere in schematic and connected with any block as signal destination. One Input Alias can have multiple output Aliases if required.
Clicking on any Input/Output Alias will highlight all aliases. All Aliases will be highlighted in “Aqua” color.
User can go to particular output alias of choice by using this option. Example: If user clicks “1” in 'Go to Alias Output' option, then 'Mute_0' block will come into visible part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.
At any time, user can navigate back to Input Alias from any Output Alias using this option. 'Goto Alias Input' option will be shown in every output alias. After clicking that option, Input Alias block will come into center part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.