This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:targetintegration [05 May 2021 13:22] – Note added John Joseph | resources:tools-software:sigmastudiov2:targetintegration [29 Apr 2022 15:26] – ADSP-21593 and ADSP-SC594 added John Joseph | ||
---|---|---|---|
Line 8: | Line 8: | ||
\\ | \\ | ||
===== Rebuild Demo Application ===== | ===== Rebuild Demo Application ===== | ||
- | The Default Application for ADSP-21489, ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-21584, and ADSP-21573, ADSP-21569 are supplied with the package. Follow the steps given below to rebuild the Application. The projects can be found under target specific subfolders inside “SigmaStudioPlus-Relx.y.z\Target\Examples\Demo”. | + | The Default Application for ADSP-21489, ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-21584, and ADSP-21573, ADSP-21569, ADSP-21593, ADSP-SC594 |
- Launch CrossCore Embedded Studio on the SigmaStudio+ Host PC. Specify the workspace when prompted. | - Launch CrossCore Embedded Studio on the SigmaStudio+ Host PC. Specify the workspace when prompted. | ||
- | - Select File-> | + | - Select File-> |
- | - Select File-> | + | - Select File-> |
- Select File-> | - Select File-> | ||
- | - Select all the three projects (SS_App_Core0, | + | - Select all the three projects (SS_App_Core0, |
- | - Select the two projects (SS_App_Core1 and SS_App_Core2). Clean and rebuild the projects in the required configuration (Release/ | + | - Select the two projects (SS_App_Core1 and SS_App_Core2). Clean and rebuild the projects in the required configuration (Release/ |
- Select the project (SS_App_Core1). Clean and rebuild the projects in the required configuration (Release/ | - Select the project (SS_App_Core1). Clean and rebuild the projects in the required configuration (Release/ | ||
- The newly generated executable(s) will be present in “Debug” or “Release” folder based on the chosen configuration. | - The newly generated executable(s) will be present in “Debug” or “Release” folder based on the chosen configuration. |