Prototype
ADI_SS_RESULT adi_ss_updateParam(ADI_SS_SSN_HANDLE hSSn, uint32_t *pParamDataAddr, uint32_t nSSnParamMemOffset, uint32_t nNumParams);
Description
This function is used to update a single or a set SS+ parameters into the SS+ parameter memory space.
Parameters
Name: hSSn Type: ADI_SS_SSN_HANDLE Direction: Input Description: Handle to the SSn instance. Name: nSSnParamMemOffset Type: uint32_t Direction: Input Description: Offset from the parameter memory base into which the new parameters need to be updated. Name: pParamDataAddr Type: uint32_t * Direction: Input Description: Pointer to memory holding the new parameter values. Name: nNumParams Type: uint32_t Direction: Input Description: Number of parameters that needs to be updated.
Return value
An appropriate error code of type ADI_SS_RESULT is returned.