This is an old revision of the document!
In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, downloading the SMAP, SS+ code and parameters on to the SHARC cores of ADSP-SC5xx.
A utility is provided with the package by which the exported code and parameters by SigmaStudio+ can be converted into a ‘C’ compiler readable form. This utility create arrays of SMAP, SS+ code and parameters as part of a ‘C’ file which can directly be included in the SigmaStudio+ ARM application for ADSP-SC5xx.