This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:support [30 Jun 2020 13:03] – page updated John Joseph | resources:tools-software:sigmastudiov2:support [13 Feb 2023 13:17] – FAQ updated John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources: | [[resources: | ||
- | =====Support===== | + | ======Support |
- | \\ | + | |
If you have a technical problem and you can't find a solution, you can contact for Technical Support by email: **ssplus_support@analog.com** | If you have a technical problem and you can't find a solution, you can contact for Technical Support by email: **ssplus_support@analog.com** | ||
+ | \\ | ||
+ | \\ | ||
+ | =====FAQ===== | ||
+ | \\ | ||
+ | ====Communication==== | ||
+ | \\ | ||
+ | **Q: Why does the readback from target fails even though the download is successful and there is audio playback? | ||
+ | \\ | ||
+ | \\ | ||
+ | A: When USBi is used as the communication device, the " | ||
+ | \\ | ||
+ | \\ | ||
+ | ====Download==== | ||
+ | \\ | ||
+ | **Q: Why does SigmaStudio+ throw " | ||
+ | \\ | ||
+ | \\ | ||
+ | A: " | ||
+ | - Target application is not loaded properly. | ||
+ | - Target is executing properly. However, SigmaStudio+ is not able to read the status of the target. | ||
+ | When USBi is used as the communication device, the " | ||
+ | \\ | ||
+ | \\ | ||
+ | ====Platform==== | ||
+ | \\ | ||
+ | **Q: Project download on to ADSP-21489 fails when the target application is loaded from serial (SPI) flash. What is the reason?** | ||
+ | \\ | ||
+ | \\ | ||
+ | A: On ADSP-21489, SPI Flash and USBi shares the same SPI lines. As a result, the SPI boot fails when USBi is connected. | ||
+ | * When SPI boot fails, LED 1-8 will be ON | ||
+ | * When SPI boot succeeds, LED 1 will be ON. LED 2-8 will be OFF. | ||
+ | Workaround is to disconnect the USBi, reset the board (then successful boot happens and LED1 will be ON). Now connect the USBi and download the project from SigmaStudio+. Upon successful download, you will find LED 1-4 ON. | ||
+ | |||
+ |