This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:sources:sweepswitch [05 May 2021 14:47] – Prasad Kamath | resources:tools-software:sigmastudiov2:modules:sources:sweepswitch [12 May 2021 12:53] – [DSP Parameters] Prasad Kamath | ||
---|---|---|---|
Line 7: | Line 7: | ||
\\ | \\ | ||
The Sweep block generates a sinewave that sweeps from a start frequency to an end frequency. The sweep rate is determined by the number of sweep steps and cycles per step. In case of the linear sweep, the frequency sweep is linear across time whereas in the case of log sweep input, the frequency sweeps logarithmically cross time. The following variants of the module are available: | The Sweep block generates a sinewave that sweeps from a start frequency to an end frequency. The sweep rate is determined by the number of sweep steps and cycles per step. In case of the linear sweep, the frequency sweep is linear across time whereas in the case of log sweep input, the frequency sweeps logarithmically cross time. The following variants of the module are available: | ||
- | * LinearSweepInput | + | * Linear Sweep Switch |
- | * LinearSweepWithInputTB | + | * Linear Sweep With Switch Tone Burst |
- | * LogSweepInput | + | * Log Sweep Switch |
- | * LogSweepWithInputTB | + | * Log Sweep With Switch Tone Burst |
\\ | \\ | ||
===== Usage ===== | ===== Usage ===== | ||
Line 47: | Line 47: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ | + | ^Parameter Name^Description^ADAU145x/146x^ |
| ----------------------------- | --------------------------------------------------------------------------------------------------- |----------------------------------------------------- | | | ----------------------------- | --------------------------------------------------------------------------------------------------- |----------------------------------------------------- | | ||
- | |start_freq|normalised value of start frequency|Float| | + | |start_freq|normalised value of start frequency|FixPoint8d24| |
- | |stop_freq|normalised value of end frequency|Float| | + | |stop_freq|normalised value of end frequency|FixPoint8d24| |
- | |numcycles_per_step|Gain, | + | |numcycles_per_step|Gain, |
- | |numsteps|number of steps between start and stop|Float| | + | |numsteps|number of steps between start and stop|Integer32| |
- | |freq_increment| frequency increment defined by range and numsteps |Float| | + | |freq_increment| frequency increment defined by range and numsteps |FixPoint8d24| |
- | |ison |Enabled/ | + | |ison |Enabled/ |
\\ | \\ | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== |