Click here to return to the Sources page
The DC Input No MIPs Block is a parameter value write utility which can write directly to any parameter.
The block's controls allow the value and the format to be set. There are 32/28 available bits which can be used to represent decimal values depends on the SigmaDSP.
Name | ADSP-214xx | ADSP-215xx/ADSP-SC5xx | ADAU145x/146x |
---|---|---|---|
—————————————- | —————————————— | ————————————————-- | ——————————————- |
DC Input No MIPs | NA | NA | Sample |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | ———————————— | ———————————————————-- |
DCValue | 0 | 0 to 2147483647 | This control gives the DC, direct current, signal(a constant numeric value) |
IntegerBits | 5/8 | 0 to 32 (Only for SigmaDSP) | This control decides the range of DC control |
DecimalBits | 23/24 | 0 to 32(Only for SigmaDSP) | This control decides the range of DC control |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————-- | ——————————————————————— | ———————————————— | ——————————— |
DCValue | DC, direct current, signal(a constant numeric value) | Float | Format specified in UI |