This is an old revision of the document!
Click here to return to the Mixers and Splitters page
The Multiple Control Splitter allows an input signal to be split into two or more outputs with independent control of each output's gain.
There is a control knob for setting the gain or each output. To set the gain, click the knob with the left mouse button and drag while holding down the button. Each knob's range, value, and step size can be customized in the control pop-up window. To change the knob settings, right-click on the knob control
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
———————————————————— | ——————-- | ——————————-- | —————————- |
Multiple Control Splitter (No Slew) | B/S | B/S | S |
Multiple Control Splitter (SW Slew) | B/S | B/S | NA |
Multiple Control Splitter (HW Slew) | NA | NA | S |
Name | Type | Description |
---|---|---|
Input | Audio | Input channel |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
OutputX | Audio | Output Channel X |
Note:
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Gain_Channel0 | 0 dB | -200 to 200 dB | Gain factor |
NumChannels | 2 | 20 | Number of output channels. Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
Gain_Channel0 | scaling of the inputs | Float |