This is an old revision of the document!
Click here to return to the Master Control Port page
There are two different versions of the SPI Read module.
The 'SPI Periodic Read' block reads a particular sub address from any SPI slave periodically and sends the value read in the output pin.
Click on to configure the parameters for SPI read.
To monitor multiple registers in the same slave, create multiple instances of the cell.
If the device to be programmed is selected through MP0 (the /SS_M pin), no configuration is required in the register controls. Otherwise, the multipurpose pin must be configured to act as the slave select in the Register Window. (Hardware Configuration → ICx - ADAU145x Register Controls → MULTIPURPOSE/AUXADC)
The following table shows the mapping between the module's parameter and the register control window. Please note that for some other blocks, there is an offset of 1 between the module parameter and the register control window.
'Slave Select' in Configuration Window | 'Slave Select Channel' in the Register control |
---|---|
0 | Slave Select Channel 0 |
1 | Slave Select Channel 1 |
2 | Slave Select Channel 2 |
3 | Slave Select Channel 3 |
4 | Slave Select Channel 4 |
5 | Slave Select Channel 5 |
Name | ADSP-214xx | ADSP-215xx/ADSP-SC5xx | ADAU145x/146x |
---|---|---|---|
—————————————- | —————————————— | ————————————————-- | ——————————————- |
SPI Periodic Read | Not Supported | Not Supported | Sample |
Name | Type | Description |
---|---|---|
————————— | ——————————- | ————————————-- |
SPI Data | Control | Outputs data read over SPI |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————————- | ———————- | —————————————— | ———————————————————————- |
SPIBitrate | 100 kHz | 100 kHZ - 100000 kHZ | SPI Speed |
SPISlaveSelectChannel | 0 | 0 – 6 | SPI Slave Select Channel |
SPIMode | SPI Mode 3 | Mode 0/ Mode 3 | SPI protocol mode |
DataLength | 4 | 1-4 | Length of the data to be read |
AddressLength | 2 | 1-4 | Length of the sub address |
Read Interval | 50 ms | 50 - 5000 ms | Interval between 2 consecutive SPI Read |
AddressToRead | 0 | 0 to Pow(2, Address Length) - 1 | Address to be read from |
SPIReadInstruction | 1 | 0-255 | Instruction value for a read operation (0x1 for ADI audio devices, typically 0x3 for eeprom/flash) |
SPICommandLength | 1 | 1-4 | Length of the command sent in bytes |
InitialOutputValue | 0 | -2147483648 to 2147483647 | Value in the output pin till the first read is complete. |
Parameter Name | Description | ADAU145x/146x | |
---|---|---|---|
—————————————- | —————————————————————————————————————————— | —————————- | |
spiSpeed | SPI Speed | Integer32 | |
spiMode | SPI Protocol Mode | Integer32 | |
slaveSelect | SPI Slave Select Channel | Integer32 | |
readAddress | Address to be read from | Integer32 | |
addressLength | Length of the sub address | Integer32 | |
dataLength | Length of the data to be read | Integer32 | |
commandLength | Length of the command sent in bytes | Integer32 | |
readInstruction | Instruction value for a read operation (0x1 for ADI audio devices, typically 0x3 for eeprom/flash) | Integer32 |
Not applicable
The 'SPI Read with external Trigger' block reads a particular sub address from any I2C slave when a rising edge is detected in the input pin.
Click on to configure the parameters for SPI read.
To monitor multiple registers in the same slave, create multiple instances of the cell.
If the device to be programmed is selected through MP0 (the /SS_M pin), no configuration is required in the register controls. Otherwise, the multipurpose pin must be configured to act as the slave select in the Register Window. (Hardware Configuration → ICx - ADAU145x Register Controls → MULTIPURPOSE/AUXADC)
The following table shows the mapping between the module's parameter and the register control window. Please note that for some other blocks, there is an offset of 1 between the module parameter and the register control window.
'Slave Select' in Configuration Window | 'Slave Select Channel' in the Register control |
---|---|
0 | Slave Select Channel 0 |
1 | Slave Select Channel 1 |
2 | Slave Select Channel 2 |
3 | Slave Select Channel 3 |
4 | Slave Select Channel 4 |
5 | Slave Select Channel 5 |
Name | ADSP-214xx | ADSP-215xx/ADSP-SC5xx | ADAU145x/146x |
---|---|---|---|
—————————————- | —————————————— | ————————————————-- | ——————————————- |
SPI Read with External Trigger | Not Supported | Not Supported | Sample |
Name | Type | Description |
---|---|---|
————————— | ——————————- | ————————————-- |
Trigger | Control | Rising edge in this signal initiates read |
Name | Type | Description |
---|---|---|
————————— | ——————————- | ————————————-- |
SPI Data | Control | Outputs data read over SPI |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————————- | ———————- | —————————————— | ———————————————————————- |
SPIBitrate | 100 kHz | 100 kHZ - 100000 kHZ | SPI Speed |
SPISlaveSelectChannel | 0 | 0 – 6 | SPI Slave Select Channel |
SPIMode | SPI Mode 3 | Mode 0/ Mode 3 | SPI protocol mode |
DataLength | 4 | 1-4 | Length of the data to be read |
AddressLength | 2 | 1-4 | Length of the sub address |
AddressToRead | 0 | 0 to Pow(2, Address Length) - 1 | Address to be read from |
SPIReadInstruction | 1 | 0-255 | Instruction value for a read operation (0x1 for ADI audio devices, typically 0x3 for eeprom/flash) |
SPICommandLength | 1 | 1-4 | Length of the command sent in bytes |
InitialOutputValue | 0 | -2147483648 to 2147483647 | Value in the output pin till the first read is complete. |
Parameter Name | Description | ADAU145x/146x | |
---|---|---|---|
—————————————- | ——————————————————————————-- | —————————- | |
spiSpeed | SPI Speed | Integer32 | |
spiMode | SPI Protocol Mode | Integer32 | |
slaveSelect | SPI Slave Select Channel | Integer32 | |
readAddress | Address to be read from | Integer32 | |
addressLength | Length of the sub address | Integer32 | |
dataLength | Length of the data to be read | Integer32 | |
commandLength | Length of the command sent in bytes | Integer32 | |
readInstruction | Instruction value for a read operation (0x1 for ADI audio devices, typically 0x3 for eeprom/flash) | Integer32 |
Not applicable