Wiki

This version is outdated by a newer approved version.DiffThis version (13 May 2021 10:24) is a draft.
Approvals: 0/1
The Previously approved version (19 Mar 2021 15:26) is available.Diff

This is an old revision of the document!


Click here to return to the IO page Click here to return to the IO page

Digital Microphone Input



Description

The Digital Microphone Input block receives input from the hardware's microphone input pins and makes it available in the schematic design.

Usage

Check the block for the input channel(s) you with to enable. Un-check the box disable an input channel. The pin will turn blue when an input is enabled and grey when disabled. The default block has two pins enabled, for stereo connection.

Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xx ADAU145x/ADAU146x
————————————————-——————————————-——————————--
Digital Microphone Input Block & Sample Block & Sample Sample


Pins

Output

NameTypeDescription
——————————-————————————-—————————--
Output0AudioMic Output channel 0
Output1AudioMic Output channel 1


Configurable Parameters


Not applicable

DSP Parameters

No DSP Parameters

resources/tools-software/sigmastudiov2/modules/inputoutput/digmicinput.1620894246.txt.gz · Last modified: 13 May 2021 10:24 by Prasad Kamath