This is an old revision of the document!
Click here to return to the Gain page
The Multiple Volume Control block allows gain adjustment to be made to each of the inputs individually.Every input pin has its own volume control.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Multiple Volume Control | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel 0 |
Name | Type | Description |
---|---|---|
Output0 | Control | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Gain_channel<n> | 0 dB | -200 to +200 dB | Increases/decreases the dB level of the input |
IsDBps_channel<n> | True | True/False | Allows to controls either in dBps/linear |
Max_Channel<n> | 0 | Min_Channel < Max_Channel < 200 | Configure the maximum value of gain for nth channel |
Min_Channel<n> | 0 | -200 < Min_Channel < Max_Channel | Configure the minimum value of gain for nth channel |
NumChannels | 1 | 20 | Num of input and output channels.Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
Gain_channel<n> | Increases/decreases the dB level of the input | Float |
Slew_Channel<n> | smootly transition of signal from one level to another level | Float |
Slew_Channel0 = 2^(-12);