This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:filters:mediumsizeeq [14 Jan 2020 11:50] – Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:filters:mediumsizeeq [15 May 2021 08:39] (current) – [DSP Parameters] Sreesha Y M | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Medium Size Eq ====== | ====== Medium Size Eq ====== | ||
+ | \\ | ||
+ | {{: | ||
+ | \\ | ||
+ | {{: | ||
===== Description ===== | ===== Description ===== | ||
This block gives access to two general 2nd-order filters: Peaking and Shelving EQ. | This block gives access to two general 2nd-order filters: Peaking and Shelving EQ. | ||
+ | \\ | ||
===== Usage ===== | ===== Usage ===== | ||
To open the filter control window, click on the icon button. Select the desired filter type from the drop-down combo-box list. The filter controls and the icon button image will change to reflect the selected filter type. | To open the filter control window, click on the icon button. Select the desired filter type from the drop-down combo-box list. The filter controls and the icon button image will change to reflect the selected filter type. | ||
+ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |Medium Size Eq| Yes | Yes|Yes| Yes| | + | | -------------------------------------- | -------------------- | -------------------------------- | ---------------------------- | |
+ | |Medium Size Eq| B/S | B/S | S | | ||
+ | |Medium Size Eq Slew| NA | NA | S | | ||
+ | |Medium Size Eq Slew Ext| NA | NA | S | | ||
+ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Input0|Audio|Input Channel 0| | |Input0|Audio|Input Channel 0| | ||
+ | |Lambda0 (For Slew Ext Only)|Control|External Slew Input for Stage 0| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------ | ------------------------------ | ------------------------------------------------ | | ||
|Output0|Audio|Output channel 0| | |Output0|Audio|Output channel 0| | ||
+ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |Boost|0 dB| -10 to +10 dB|Set the boost value for a particular filter curve| | + | |----------------------------------------------------------|---------------------------|---------------------------------------------|----------------------------------------------------------| |
- | |Frequency|1000|0 to 96000Hz|Cut-off frequency| | + | |Stage< |
- | |Gain|0 dB|-15 to +15 dB|Filter Gain| | + | |Stage<fc # |
- | |Q|1.41|0.1 to 16|Q factor of the filter| | + | |Stage<fc # |
- | |Slope|1|0 to 2|Slope controls filter steepness and therefore the transition between the boost/cut and the flat response.| | + | |Stage<fc # |
- | |FilterType|Parametric filter|Available filter Types|Controls the type of the filter| | + | |Stage<fc # |
- | |EnabledOrBypassed|True|True/ | + | |Stage<fc # |
- | |Phase|False|True/ | + | |Stage<fc # |
- | |LockFrequency|False|True/ | + | |Stage<fc # |
+ | |Stage<fc # | ||
+ | |Stage< | ||
|NumStages|1|1 to 20 | Number of stages of filter. Change in this value requires re-compilation| | |NumStages|1|1 to 20 | Number of stages of filter. Change in this value requires re-compilation| | ||
|NumChannels|1| 1 to 20|Number of input and output channels. Change in this value requires re-compilation| | |NumChannels|1| 1 to 20|Number of input and output channels. Change in this value requires re-compilation| | ||
+ | |SlewType (For Slew Variant ADAU145x/ | ||
+ | |CustomSlew (For Slew Variant ADAU145x/ | ||
+ | \\ | ||
+ | Here, * <fc #ff0000> X</ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^ Parameter Name |
- | |Stage< | + | | ------------------------------------ | --------------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | |
- | |Stage< | + | |Stage< |
- | |Stage< | + | |Stage< |
- | |Stage< | + | |Stage< |
- | |Stage< | + | |Stage< |
+ | |Stage< | ||
+ | |slew_mode |Slew value for medium size eq slew variant only | NA | Integer32 | | ||
+ | |Stage< | ||
\\ Here, | \\ Here, | ||
- | * <fc # | + | * <fc # |
\\ | \\ |