This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:filters:adaptivemfxlmsfilter [16 May 2021 10:14] – [Configurable Parameters] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:filters:adaptivemfxlmsfilter [16 May 2021 10:18] (current) – Nikhin Shetty | ||
---|---|---|---|
Line 19: | Line 19: | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | ---------------------- | ------------------------ | --------------------------------------------------------------------------------------- | | + | | ---------------------- | -------------- | ---------------------- | |
|Input< | |Input< | ||
|ErrorIN< | |ErrorIN< | ||
Line 28: | Line 28: | ||
| ---------------------- | -------------- | ---------------------- | | | ---------------------- | -------------- | ---------------------- | | ||
|Output< | |Output< | ||
- | |ErrorOUT< | + | |ErrorOUT< |
Note: | Note: | ||
* <fc # | * <fc # | ||
Line 36: | Line 36: | ||
===Sec Path Training === | ===Sec Path Training === | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | | ---------------------------------------- | ---------------------- | -------------------------------- | ---------------------------------------- | | + | | ---------------------------------------- | ---------------------- | ------------------------------------------ | ------------------------------------------------------------------------------ | |
|Current Output| 0 | 0 to OutputChannel Count - 1|Output selection for which secondary paths are to be estimated | | |Current Output| 0 | 0 to OutputChannel Count - 1|Output selection for which secondary paths are to be estimated | | ||
|Step Size| 0.9 |0.000001- 0.999999 | Secondary path LMS filter step size | | |Step Size| 0.9 |0.000001- 0.999999 | Secondary path LMS filter step size | | ||
Line 45: | Line 45: | ||
===RunTime === | ===RunTime === | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | | ---------------------------------------- | ---------------------- | -------------------------------- | ---------------------------------------- | | + | | ---------------------------------------- | ---------------------- | ------------------------------------------ | ------------------------------------------------------------------------------ | |
|Filter Length| 32 | 8 to 256 |MFXLMS Filter length | |Filter Length| 32 | 8 to 256 |MFXLMS Filter length | ||
|Step Size| 0.9 |0.000001- 0.999999 | LMS step size | | |Step Size| 0.9 |0.000001- 0.999999 | LMS step size | |