This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:signalenvelope [27 Feb 2020 05:44] Krithika Manchale [Description] |
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:signalenvelope [12 May 2021 09:37] John Joseph |
||
---|---|---|---|
Line 1: | Line 1: | ||
- | [[resources/tools-software/sigmastudiov2/modules/dynamicprocessors|Click here to return to the Dynamic Processors page]] | + | [[resources/tools-software/sigmastudiov2/modules/dynamicsprocessors|Click here to return to the Dynamic Processors page]] |
====== Signal Envelope ====== | ====== Signal Envelope ====== | ||
\\ | \\ | ||
Line 7: | Line 7: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)^ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ |
- | |Signal Envelope| Yes | Yes|Yes| Yes| | + | | --------------------------------------------- | ---------------------------- | -------------------------------- | ---------------------------- | |
+ | | Signal Envelope | B/S | B/S | B/S | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Input|Audio|Input channel| | |Input|Audio|Input channel| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Output|Audio|Output channel| | |Output|Audio|Output channel| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | | ---------------------------------------------- | ---------------------------- | ------------------------------------- |---------------------------------------------------------------- | | ||
|RmsTC|120|1 to 10000| Controls the time constant (TC) in dB/second that is used for calculating the RMS input value. The time constant determines how rapidly the compressor will respond to input signal level changes, e.g. the “Attack” time.| | |RmsTC|120|1 to 10000| Controls the time constant (TC) in dB/second that is used for calculating the RMS input value. The time constant determines how rapidly the compressor will respond to input signal level changes, e.g. the “Attack” time.| | ||
|Hold|0|0 to 2000| Controls the time (ms)the envelope maintains the output level before it starts decreasing as the input level decreases| | |Hold|0|0 to 2000| Controls the time (ms)the envelope maintains the output level before it starts decreasing as the input level decreases| | ||
Line 25: | Line 29: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ | + | ^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ ADAU145x/146x ^ |
- | |RmsTC|Controls the time constant (TC) in dB/second that is used for calculating the RMS input value.|Float| | + | |------------------------|------------------------------------------------------------------------------------- |-------------------------------------------| ---------------------------------------------- | |
- | |Hold|Controls the time (ms)the envelope maintains the output level before it starts decreasing as the input level decreases|Float| | + | |RmsTC|Controls the time constant (TC) in dB/second that is used for calculating the RMS input value.|Float| 8.24 format| |
- | |Decay|Controls the rate at which envelope signal decreases in response to the decrease in the input signal|Float| | + | |Hold|Controls the time (ms)the envelope maintains the output level before it starts decreasing as the input level decreases|Float| 8.24 format| |
+ | |Decay|Controls the rate at which envelope signal decreases in response to the decrease in the input signal|Float| 8.24 format| | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== |