This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:rmswithexternalinput [14 Jan 2020 08:14] – [DSP Parameter Computation] Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:rmswithexternalinput [28 Sep 2023 10:08] (current) – [Configurable Parameters] Arpit Arora | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | [[resources/ | + | [[resources/ |
====== RMS w/Ext Detector ====== | ====== RMS w/Ext Detector ====== | ||
+ | \\ | ||
+ | {{: | ||
+ | \\ | ||
+ | {{: | ||
===== Description ===== | ===== Description ===== | ||
The RMS w/Ext Detector Compressor block computes the RMS level of the control signal and applies the compressor gain to the input signal based on the RMS value. | The RMS w/Ext Detector Compressor block computes the RMS level of the control signal and applies the compressor gain to the input signal based on the RMS value. | ||
+ | \\ | ||
+ | ===== Variants ===== | ||
+ | - RMS w/Ext Detector | ||
+ | - RMS w/Ext Detector Input and Gain Out | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name |
- | |RMS w/Ext Detector| | + | | ------------------------------------------------------ | --------------------------- | -----------------------------| ---------------------------- | |
+ | | RMS w/Ext Detector | B/S | B/S | S | | ||
+ | | RMS w/Ext Detector Input and Gain Out| NA | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|ExtDetectorInput|Control|Determines the amount of compressor gain applied to the input signal| | |ExtDetectorInput|Control|Determines the amount of compressor gain applied to the input signal| | ||
|Input1|Audio|Input channel1| | |Input1|Audio|Input channel1| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Output1|Audio|Output channel1| | |Output1|Audio|Output channel1| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |TimeConstant|121| 1 to 8686 dB/ | + | | ---------------------------------------------- |
+ | |TimeConstant|121| 1 to 10000 dB/ | ||
|Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | |Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | ||
|Decay| 10 dB/s| 0 to 10000 dB/ | |Decay| 10 dB/s| 0 to 10000 dB/ | ||
- | |SoftKnee|False|True/ | + | |SoftKnee|False|True/ |
|Table|All values are 1|-|Table values are the gain points used to apply for input signal level| | |Table|All values are 1|-|Table values are the gain points used to apply for input signal level| | ||
- | |IsDBps|True|True/ | + | |IsDBps|True|True/ |
|NumChannels|1|1 to 20|Number of input and output channels. Change in this value requires re-compilation| | |NumChannels|1|1 to 20|Number of input and output channels. Change in this value requires re-compilation| | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^Description^ADSP-214xx/ |
- | |TimeConstant|RMS time constant value|Float| | + | |------------------------------ |------------------------------------------ |------------------------------------------| ---------------------------------------------- | |
- | |Hold|Hold value|Float| | + | |TimeConstant|RMS time constant value|Float| 8.24 format| |
- | |Decay|Decay value|Float| | + | |Hold|Hold value|Float| 8.24 format| |
- | |Table|Table values | Float| | + | |Decay|Decay value|Float| 8.24 format| |
- | |LogCoeff| Constant coefficients|Float| | + | |Table|Table values | Float| 8.24 format| |
+ | |LogCoeff| Constant coefficients|Float| 8.24 format| | ||
+ | \\ | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== | ||
\\ | \\ |