This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:peakcompressor [15 Jan 2021 10:59] – [Peak Compressor] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:peakcompressor [12 May 2021 09:35] (current) – John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | [[resources/ | + | [[resources/ |
====== Peak Compressor ====== | ====== Peak Compressor ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
\\ | \\ | ||
{{: | {{: | ||
===== Description ===== | ===== Description ===== | ||
The Peak Compressor block computes the peak level of the input signal, if peak of the signal is more than the threshold level, signal level immediately changes to new peak level and if the peak level is below the threshold level, it slowly reaches the new peak level by accounting to the hold and decay time. | The Peak Compressor block computes the peak level of the input signal, if peak of the signal is more than the threshold level, signal level immediately changes to new peak level and if the peak level is below the threshold level, it slowly reaches the new peak level by accounting to the hold and decay time. | ||
+ | \\ | ||
+ | ===== Variants ===== | ||
+ | - Peak Compressor | ||
+ | - Peak Compressor with Gain Out | ||
+ | |||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name |
- | |Peak Compressor| | + | | -------------------------------------------------------- | ---------------------------- | -------------------------------- | ---------------------------- | |
+ | | Peak Compressor | B/S | ||
+ | | Peak Compressor with Gain Out | NA | NA | S | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Input1|Audio|Input channel1| | |Input1|Audio|Input channel1| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | --------------------------------------- | ------------------------------ | ------------------------------------------------ | | ||
|Output1|Audio|Output channel1| | |Output1|Audio|Output channel1| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | | ---------------------------------------------- | ||
|Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | |Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output | ||
|Decay| 10 dB/s| 0 to 10000 dB/ | |Decay| 10 dB/s| 0 to 10000 dB/ | ||
Line 30: | Line 41: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^Description^ADSP-214xx/ |
- | |Hold|Hold value|Float| | + | |------------------------------ |------------------------------------------ |-------------------------------------------| ---------------------------------------------- | |
- | |Decay|Decay value|Float| | + | |Hold|Hold value|Float| 8.24 format| |
- | |Table|Table values | Float| | + | |Decay|Decay value|Float| 8.24 format| |
+ | |Table|Table values | Float| 8.24 format| | ||
\\ | \\ | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== |