This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:basic:stopwatch [14 Jan 2021 17:49] – [Stop Watch] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:stopwatch [10 May 2021 09:26] (current) – [Input] Nikhin Shetty | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Stop Watch ====== | ====== Stop Watch ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
\\ | \\ | ||
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
The StopWatch block is used to know how long something takes (i.e. how many samples have passed between start and stop event). A control signal greater than zero to Start pin triggers the Stopwatch counter, While the control signal to Stop pin is zero. A control signal greater than zero to Stop pin stops the counter increment regardless of the control signal to the Start pin. Reset button(pin for External Reset, the control signal is high) resets the counter value to zero. | The StopWatch block is used to know how long something takes (i.e. how many samples have passed between start and stop event). A control signal greater than zero to Start pin triggers the Stopwatch counter, While the control signal to Stop pin is zero. A control signal greater than zero to Stop pin stops the counter increment regardless of the control signal to the Start pin. Reset button(pin for External Reset, the control signal is high) resets the counter value to zero. | ||
Line 13: | Line 13: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |StopWatch| Yes | Yes|Yes| Yes| | + | | ------------------------------------------------------------ |
- | |StopWatchExtReset| | + | |StopWatch| B/S | B/S | S | |
+ | |StopWatchExtReset| | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Start|Control|Starts the counter of the stop watch| | + | |-------------------------------------------------------|------------------------------------------------------------|------------------------------| |
- | |Stop|Control|Stops the counter of the stop watch| | + | |Start | Audio | Starts the counter of the stop watch| |
- | |Reset|Control|Resets the counter of the stop watch (only for StopWatchExtReset)| | + | |Stop | Audio | Stops the counter of the stop watch| |
+ | |Reset | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Counter|Control|Stop Watch counter output| | + | |------------------------------|------------------------------------------------------------|------------------------------| |
+ | |Output| Control | Stop Watch counter output| | ||
\\ | \\ | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |Reset|False| True/ | + | |------------------------------|---------------------------|----------------------------|----------------------------------------------------------| |
+ | |Reset | False | True / False | Resets the counter value to zero (Only for StopWatch) | | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^ Parameter Name |
- | |Reset|Resets the counter result to zero (Only for StopWatch) |Float| | + | | ---------------------------------------- | -------------------------------------------------------------------------------- | ---------------------------------------- | ---------------------------- | |
+ | |Reset| Resets the counter result to zero (Only for StopWatch) | Float| FixPoint8d24 | ||
\\ | \\ | ||